CameraCollection Class¶
-
class
NXOpen.Display.
CameraCollection
¶ Bases:
object
Represents a collection cameras
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CreateCameraBuilder | Creates a NXOpen.Display.CameraBuilder object if camera is None. |
FindObject | Finds the NXOpen.Display.Camera with the given identifier as recorded in a journal. |
Method Detail¶
CreateCameraBuilder¶
-
CameraCollection.
CreateCameraBuilder
¶ Overloaded method CreateCameraBuilder
CreateCameraBuilder(camera)
CreateCameraBuilder(view, layout, camera)
-------------------------------------
Creates a
NXOpen.Display.CameraBuilder
object if camera is None. Otherwise, a Camera object will be editedSignature
CreateCameraBuilder(camera)
Parameters: camera ( NXOpen.Display.Camera
) – If camera is not None, then this object will be editedReturns: return camera builder Return type: NXOpen.Display.CameraBuilder
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Creates a
NXOpen.Display.CameraBuilder
object if camera is None. Otherwise, a Camera object will be edited. Initializes the camera with data from the view in the layoutSignature
CreateCameraBuilder(view, layout, camera)
Parameters: - view (
NXOpen.View
) – Use this view’s data to initialize the camera - layout (
NXOpen.Layout
) – Layout of the view - camera (
NXOpen.Display.Camera
) – If camera is not None, then this object will be edited
Returns: return camera builder
Return type: New in version NX6.0.0.
License requirements: None.
-------------------------------------
FindObject¶
-
CameraCollection.
FindObject
¶ Finds the
NXOpen.Display.Camera
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: Camera found Return type: NXOpen.Display.Camera
New in version NX5.0.0.
License requirements: None.