BoundedGridBuilder Class¶
-
class
NXOpen.Display.
BoundedGridBuilder
¶ Bases:
NXOpen.Display.GridBuilder
Represents the builder for creating a bounded grid
NXOpen.Display.BoundedGrid
.This is an abstract class, and cannot be instantiated.
Default values.
Property Value SectionCurveSettings.ColorOption Any SectionCurveSettings.Show false New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Associative | Returns or sets the associative |
LabelReference | Returns or sets the label reference |
LineColor | Returns or sets the line color |
LocalOrigin | Returns or sets the local origin |
MajorLineSpacing | Returns or sets the major line spacing |
MajorLineStyle | Returns or sets the major line style |
MajorLineWeight | Returns or sets the major line weight |
MinorLineStyle | Returns or sets the minor line style |
MinorLineWeight | Returns or sets the minor line weight |
MinorLinesPerMajor | Returns or sets the minor lines per major |
SectionCurveSettings | Returns the curve settings builder |
Show | Returns or sets the show |
ShowLabel | Returns or sets the show labels |
ShowMajorLines | Returns or sets the show major lines |
ShowOnTop | Returns or sets the show on top |
SnapPointsPerMinor | Returns or sets the snap points per minor |
SnapToGrid | Returns or sets the snap to grid |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCornerPoints | Gets corner points of the grid @return Flag indicating whether the corner points are valid |
GetObject | Returns the object currently being edited by this builder. |
InheritSettings | Inherits the settings from the specified grid. |
SaveCurves | Creates curves by intersecting the bounded grid with all bodies in the part of the grid object. |
SetCornerPoints | Sets corner points of the grid @return Flag indicating whether the corner points are valid |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BoundedGridBuilderLabelReferenceType Enumeration | Specifies label reference. |
BoundedGridBuilderShowLabelType Enumeration | Specifies label option to be used for grid label display. |
Property Detail¶
Associative¶
-
BoundedGridBuilder.
Associative
¶ Returns or sets the associative
-------------------------------------
Getter Method
Signature
Associative()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative(associative)
Parameters: associative (bool) – New in version NX6.0.0.
License requirements: None.
LabelReference¶
-
BoundedGridBuilder.
LabelReference
¶ Returns or sets the label reference
-------------------------------------
Getter Method
Signature
LabelReference()
Returns: Return type: NXOpen.Display.BoundedGridBuilderLabelReferenceType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LabelReference(labelReference)
Parameters: labelReference ( NXOpen.Display.BoundedGridBuilderLabelReferenceType
) –New in version NX6.0.0.
License requirements: None.
LocalOrigin¶
-
BoundedGridBuilder.
LocalOrigin
¶ Returns or sets the local origin
-------------------------------------
Getter Method
Signature
LocalOrigin()
Returns: Return type: NXOpen.Point3d
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocalOrigin(localOrigin)
Parameters: localOrigin ( NXOpen.Point3d
) – Label originNew in version NX6.0.0.
License requirements: None.
SectionCurveSettings¶
-
BoundedGridBuilder.
SectionCurveSettings
¶ Returns the curve settings builder
-------------------------------------
Getter Method
Signature
SectionCurveSettings()
Returns: Return type: NXOpen.Display.SectionCurveSettingsBuilder
New in version NX6.0.0.
License requirements: None.
ShowLabel¶
-
BoundedGridBuilder.
ShowLabel
¶ Returns or sets the show labels
-------------------------------------
Getter Method
Signature
ShowLabel()
Returns: Return type: NXOpen.Display.BoundedGridBuilderShowLabelType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowLabel(showLabelType)
Parameters: showLabelType ( NXOpen.Display.BoundedGridBuilderShowLabelType
) –New in version NX6.0.0.
License requirements: None.
Method Detail¶
GetCornerPoints¶
-
BoundedGridBuilder.
GetCornerPoints
¶ Gets corner points of the grid
Signature
GetCornerPoints()
Returns: a tuple Return type: A tuple consisting of (validCornerPoints, point1, point2, point3, point4). validCornerPoints is a bool. Flag indicating whether the corner points are valid point1 is a NXOpen.Point3d
. First corner point point2 is aNXOpen.Point3d
. Second corner point point3 is aNXOpen.Point3d
. Third corner point point4 is aNXOpen.Point3d
. Fourth corner pointNew in version NX6.0.0.
License requirements: None.
SaveCurves¶
-
BoundedGridBuilder.
SaveCurves
¶ Creates curves by intersecting the bounded grid with all bodies in the part of the grid object.
The bodies that are visible in the work view are intersected. The curves are added to the group created with the specified name. The group is displayed in the part navigator. The curves are created in the work part. These curves are not associated with the grid. These are just snapshot curves that can be used for modeling purposes. If the customer default “Load Solids/Sheets when Saving Section Curves” is enabled, the Save Copy of Section Curves command in the datum plane grid dialog will cause solid/sheet bodies to be loaded into memory for any visible lightweight bodies on the section plane. This may increase the time and memory used by the operation, but will ensure fully accurate section curves.
Signature
SaveCurves(groupName)
Parameters: groupName (str) – Name of the group containing curves. If None, a default name will be used. NOTE: The full Unicode character set is not supported for this parameter. New in version NX6.0.0.
License requirements: None.
SetCornerPoints¶
-
BoundedGridBuilder.
SetCornerPoints
¶ Sets corner points of the grid
Signature
SetCornerPoints(point1, point2, point3, point4)
Parameters: - point1 (
NXOpen.Point3d
) – First corner point - point2 (
NXOpen.Point3d
) – Second corner point - point3 (
NXOpen.Point3d
) – Third corner point - point4 (
NXOpen.Point3d
) – Fourth corner point
Returns: Flag indicating whether the
corner points are valid :rtype: bool
New in version NX6.0.0.
License requirements: None.
- point1 (
Validate¶
-
BoundedGridBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.