BoundedGridBuilderShowLabelType Enumeration¶
NXOpen.Display.BoundedGridBuilder.ShowLabelType is an alias for NXOpen.Display.BoundedGridBuilderShowLabelType
-
class
NXOpen.Display.
BoundedGridBuilderShowLabelType
¶ Bases:
object
Specifies label option to be used for grid label display.
Enum Members
orientation is aligned with the view orientation “
“None”, ” Never show labels “-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-