WireTool Class¶
-
class
NXOpen.CAM.
WireTool
¶ Bases:
NXOpen.CAM.ToolBuilder
Represents a Wire Tool
To create a new instance of this class, use
NXOpen.CAM.NCGroupCollection.CreateWireTool
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AdjReg | Returns the Adjust Register |
ChannelName | Returns or sets the channel’s name |
CutcomReg | Returns the Cutcom Register |
CutterExportBuilder | Returns the cutter export builder |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
Diameter | Returns the Tool Diameter (inheritable double) |
EndUdeSet | Returns the end ude set |
HolderDescription | Returns or sets the holder description |
HolderLibraryReference | Returns or sets the holder libref |
LibraryParametersBuilder | Returns the Library Data Object |
OptimizationMethod | Returns or sets the optim method |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
TlCtlgNum | Returns or sets the Catalog Number |
TlDescription | Returns or sets the Cutter Description |
TlHolderNumberBuilder | Returns the Holder Number |
TlLibref | Returns or sets the Cutter Libref |
TlManualToolChange | Returns or sets the Manual Tool Change |
TlNumberBuilder | Returns the Tool Number |
TlText | Returns or sets the tool text |
WireGuideList | Returns the wire guide list |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateWireGuide | Create a wire guide @return the wire guide object |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetMaterial | Get tool material @return |
GetMaterialData | Get material data |
GetObject | Returns the object currently being edited by this builder. |
SetMaterial | Set tool material |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AdjReg¶
-
WireTool.
AdjReg
¶ Returns the Adjust Register
-------------------------------------
Getter Method
Signature
AdjReg()
Returns: Return type: NXOpen.CAM.InheritableIntBuilder
New in version NX9.0.0.
License requirements: None.
CutcomReg¶
-
WireTool.
CutcomReg
¶ Returns the Cutcom Register
-------------------------------------
Getter Method
Signature
CutcomReg()
Returns: the tool cutcom register value Return type: NXOpen.CAM.InheritableIntBuilder
New in version NX9.0.0.
License requirements: None.
Diameter¶
-
WireTool.
Diameter
¶ Returns the Tool Diameter (inheritable double)
-------------------------------------
Getter Method
Signature
Diameter()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
WireGuideList¶
-
WireTool.
WireGuideList
¶ Returns the wire guide list
-------------------------------------
Getter Method
Signature
WireGuideList()
Returns: Return type: NXOpen.CAM.WireGuideList
New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
CreateWireGuide¶
-
WireTool.
CreateWireGuide
¶ Create a wire guide
Signature
CreateWireGuide()
Returns: the wire guide object Return type: NXOpen.CAM.WireGuide
New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
Validate¶
-
WireTool.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.