ToolBuilder Class¶
-
class
NXOpen.CAM.
ToolBuilder
¶ Bases:
NXOpen.CAM.NCGroupBuilder
Represents a Tool Builder
This is an abstract class, and cannot be instantiated.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ChannelName | Returns or sets the channel’s name |
CutterExportBuilder | Returns the cutter export builder |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndUdeSet | Returns the end ude set |
HolderDescription | Returns or sets the holder description |
HolderLibraryReference | Returns or sets the holder libref |
LibraryParametersBuilder | Returns the Library Data Object |
OptimizationMethod | Returns or sets the optim method |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
TlCtlgNum | Returns or sets the Catalog Number |
TlDescription | Returns or sets the Cutter Description |
TlHolderNumberBuilder | Returns the Holder Number |
TlLibref | Returns or sets the Cutter Libref |
TlManualToolChange | Returns or sets the Manual Tool Change |
TlNumberBuilder | Returns the Tool Number |
TlText | Returns or sets the tool text |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetMaterial | Get tool material @return |
GetMaterialData | Get material data |
GetObject | Returns the object currently being edited by this builder. |
SetMaterial | Set tool material |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ChannelName¶
-
ToolBuilder.
ChannelName
¶ Returns or sets the channel’s name
-------------------------------------
Getter Method
Signature
ChannelName()
Returns: The channel’s name Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ChannelName(name)
Parameters: name (str) – the channel’s name New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CutterExportBuilder¶
-
ToolBuilder.
CutterExportBuilder
¶ Returns the cutter export builder
-------------------------------------
Getter Method
Signature
CutterExportBuilder()
Returns: Return type: NXOpen.CAM.CutterExport
New in version NX9.0.1.
License requirements: None.
HolderDescription¶
-
ToolBuilder.
HolderDescription
¶ Returns or sets the holder description
-------------------------------------
Getter Method
Signature
HolderDescription()
Returns: the tool holder description value Return type: str New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
HolderDescription(holderDescriptionValue)
Parameters: holderDescriptionValue (str) – the tool holder description value New in version NX7.5.1.
License requirements: cam_base (“CAM BASE”)
HolderLibraryReference¶
-
ToolBuilder.
HolderLibraryReference
¶ Returns or sets the holder libref
-------------------------------------
Getter Method
Signature
HolderLibraryReference()
Returns: the tool holder library reference value Return type: str New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
HolderLibraryReference(holderLibrefValue)
Parameters: holderLibrefValue (str) – the tool holder library reference value New in version NX7.5.1.
License requirements: cam_base (“CAM BASE”)
LibraryParametersBuilder¶
-
ToolBuilder.
LibraryParametersBuilder
¶ Returns the Library Data Object
-------------------------------------
Getter Method
Signature
LibraryParametersBuilder()
Returns: Return type: NXOpen.CAM.Ude
New in version NX9.0.0.
License requirements: None.
TlCtlgNum¶
-
ToolBuilder.
TlCtlgNum
¶ Returns or sets the Catalog Number
-------------------------------------
Getter Method
Signature
TlCtlgNum()
Returns: the catalog number value Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TlCtlgNum(tlCtlgNumValue)
Parameters: tlCtlgNumValue (str) – the catalog number value New in version NX5.0.0.
License requirements: None.
TlDescription¶
-
ToolBuilder.
TlDescription
¶ Returns or sets the Cutter Description
-------------------------------------
Getter Method
Signature
TlDescription()
Returns: the cutter description value Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TlDescription(tlDescriptionValue)
Parameters: tlDescriptionValue (str) – the cutter description value New in version NX5.0.0.
License requirements: None.
TlHolderNumberBuilder¶
-
ToolBuilder.
TlHolderNumberBuilder
¶ Returns the Holder Number
-------------------------------------
Getter Method
Signature
TlHolderNumberBuilder()
Returns: Return type: NXOpen.CAM.InheritableIntBuilder
New in version NX5.0.0.
License requirements: None.
TlLibref¶
-
ToolBuilder.
TlLibref
¶ Returns or sets the Cutter Libref
-------------------------------------
Getter Method
Signature
TlLibref()
Returns: the cutter libref value Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TlLibref(tlLibRef)
Parameters: tlLibRef (str) – the cutter libref value New in version NX5.0.0.
License requirements: None.
TlManualToolChange¶
-
ToolBuilder.
TlManualToolChange
¶ Returns or sets the Manual Tool Change
-------------------------------------
Getter Method
Signature
TlManualToolChange()
Returns: the manual tool change value Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TlManualToolChange(tlManualToolChangeValue)
Parameters: tlManualToolChangeValue (bool) – the manual tool change value New in version NX5.0.0.
License requirements: None.
TlNumberBuilder¶
-
ToolBuilder.
TlNumberBuilder
¶ Returns the Tool Number
-------------------------------------
Getter Method
Signature
TlNumberBuilder()
Returns: Return type: NXOpen.CAM.InheritableIntBuilder
New in version NX5.0.0.
License requirements: None.
TlText¶
-
ToolBuilder.
TlText
¶ Returns or sets the tool text
-------------------------------------
Getter Method
Signature
TlText()
Returns: the tool text value Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TlText(tlText)
Parameters: tlText (str) – the tool text value New in version NX5.0.0.
License requirements: None.
Method Detail¶
GetMaterial¶
-
ToolBuilder.
GetMaterial
¶ Get tool material
Signature
GetMaterial()
Returns: Return type: str New in version NX8.0.1.
License requirements: None.
GetMaterialData¶
-
ToolBuilder.
GetMaterialData
¶ Get material data
Signature
GetMaterialData()
Returns: a tuple Return type: A tuple consisting of (libRef, name, description, code). libRef is a str. name is a str. description is a str. code is a str. New in version NX8.0.2.
License requirements: None.
SetMaterial¶
-
ToolBuilder.
SetMaterial
¶ Set tool material
Signature
SetMaterial(libRef)
Parameters: libRef (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX8.0.1.
License requirements: cam_base (“CAM BASE”)
Validate¶
-
ToolBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.