TurnConcaveCornerControl Class¶
-
class
NXOpen.CAM.
TurnConcaveCornerControl
¶ Bases:
NXOpen.TaggedObject
Represents a concave corner ja
New in version NX6.0.2.
Properties¶
Property | Description |
---|---|
Radius | Returns or sets the Concave Corner Control radius |
RadiusOption | Returns or sets the Concave Corner Control radius option |
Tag | Returns the Tag for this object. |
Type | Returns or sets the Concave Corner Control type |
Methods¶
Enumerations¶
TurnConcaveCornerControlRadiusOptions Enumeration | the Concave Corner Control radius options |
TurnConcaveCornerControlTypes Enumeration | the Concave Corner Control types |
Property Detail¶
Radius¶
-
TurnConcaveCornerControl.
Radius
¶ Returns or sets the Concave Corner Control radius
-------------------------------------
Getter Method
Signature
Radius()
Returns: the Concave Corner Control radius Return type: float New in version NX6.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Radius(radius)
Parameters: radius (float) – the Concave Corner Control radius New in version NX6.0.2.
License requirements: cam_base (“CAM BASE”)
RadiusOption¶
-
TurnConcaveCornerControl.
RadiusOption
¶ Returns or sets the Concave Corner Control radius option
-------------------------------------
Getter Method
Signature
RadiusOption()
Returns: the Concave Corner Control radius option Return type: NXOpen.CAM.TurnConcaveCornerControlRadiusOptions
New in version NX6.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadiusOption(radiusOption)
Parameters: radiusOption ( NXOpen.CAM.TurnConcaveCornerControlRadiusOptions
) – the Concave Corner Control radius optionNew in version NX6.0.2.
License requirements: cam_base (“CAM BASE”)
Type¶
-
TurnConcaveCornerControl.
Type
¶ Returns or sets the Concave Corner Control type
-------------------------------------
Getter Method
Signature
Type()
Returns: the Concave Corner Control type Return type: NXOpen.CAM.TurnConcaveCornerControlTypes
New in version NX6.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(cornerType)
Parameters: cornerType ( NXOpen.CAM.TurnConcaveCornerControlTypes
) – the Concave Corner Control typeNew in version NX6.0.2.
License requirements: cam_base (“CAM BASE”)