TurnConcaveCornerControlTypes Enumeration¶
NXOpen.CAM.TurnConcaveCornerControl.Types is an alias for NXOpen.CAM.TurnConcaveCornerControlTypes
-
class
NXOpen.CAM.
TurnConcaveCornerControlTypes
¶ Bases:
object
the Concave Corner Control types
New in version NX6.0.2.
Enum Members
Enum Member Enum Member Description ExtendTangents Concave Corner Control Type is Extend.Round Concave Corner Control Type is Round.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-