MillToolBuilder Class¶
-
class
NXOpen.CAM.
MillToolBuilder
¶ Bases:
NXOpen.CAM.MillingToolBuilder
Represents a Mill Tool Builder
To create a new instance of this class, use
NXOpen.CAM.NCGroupCollection.CreateMillToolBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ChamferLengthBuilder | Returns the Chamfer Length (inheritable double) |
ChannelName | Returns or sets the channel’s name |
CoolantThrough | Returns or sets the coolant through parameter |
CutterExportBuilder | Returns the cutter export builder |
CutterSubtype | Returns or sets the cutter subtypes |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndUdeSet | Returns the end ude set |
HelicalDiameter | Returns the helical diameter |
HelicalRampAngle | Returns the ramp angle |
HolderDescription | Returns or sets the holder description |
HolderLibraryReference | Returns or sets the holder libref |
HolderSectionBuilder | Returns the holder sections builder |
LibraryParametersBuilder | Returns the Library Data Object |
MaxCutWidth | Returns the max cut width |
MillingTrackpointBuilder | Returns the mill trackpoint builder |
MinRampLength | Returns the min ramp length |
OptimizationMethod | Returns or sets the optim method |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
TaperedShankDiameterBuilder | Returns the tapered shank diameter |
TaperedShankLengthBuilder | Returns the tapered shank length |
TaperedShankTaperLengthBuilder | Returns the tapered shank taper length |
TlAdjRegBuilder | Returns the Adjust Register |
TlCor1RadBuilder | Returns the Lower Radius builder (inheritable double) |
TlCor2RadBuilder | Returns the Upper Radius builder (inheritable double) |
TlCtlgNum | Returns or sets the Catalog Number |
TlCutcomReg | Returns or sets the Cutcom Register |
TlCutcomRegBuilder | Returns the Cutcom Register Builder |
TlDescription | Returns or sets the Cutter Description |
TlDiameterBuilder | Returns the Tool Diameter builder (inheritable double) |
TlDirection | Returns or sets the tool direction |
TlFluteLnBuilder | Returns the flute length |
TlHeightBuilder | Returns the length |
TlHolderDescription | Returns or sets the Holder Description |
TlHolderLibref | Returns or sets the Holder Library Reference |
TlHolderNumberBuilder | Returns the Holder Number |
TlLibref | Returns or sets the Cutter Libref |
TlLowCorRadBuilder | Returns the low corner radius |
TlManualToolChange | Returns or sets the Manual Tool Change |
TlNumFlutesBuilder | Returns the Number of Flutes builder (inheritable integer) |
TlNumberBuilder | Returns the Tool Number |
TlShankDiaBuilder | Returns the Shank Diameter builder (inheritable double) |
TlTaperAngBuilder | Returns the Taper Angle builder (inheritable double) |
TlText | Returns or sets the tool text |
TlTipAngBuilder | Returns the Tip Angle builder (inheritable double) |
TlUpCorRadBuilder | Returns the up corner radius |
TlXcenCor1Builder | Returns the X Center R1 builder (inheritable double) |
TlXcenCor2Builder | Returns the X Center R2 builder (inheritable double) |
TlYcenCor1Builder | Returns the Y Center R1 builder (inheritable double) |
TlYcenCor2Builder | Returns the Y Center R2 builder (inheritable double) |
TlZMountBuilder | Returns the Z Mount builder (inheritable double) |
TlZOffsetBuilder | Returns the Z Offset builder (inheritable double) |
UseTaperedShank | Returns or sets the use tapered shank |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetMaterial | Get tool material @return |
GetMaterialData | Get material data |
GetObject | Returns the object currently being edited by this builder. |
SetMaterial | Set tool material |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MillToolBuilderCutterSubtypes Enumeration | Available types for mill tool subtype |
Property Detail¶
ChamferLengthBuilder¶
-
MillToolBuilder.
ChamferLengthBuilder
¶ Returns the Chamfer Length (inheritable double)
-------------------------------------
Getter Method
Signature
ChamferLengthBuilder()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX8.0.0.
License requirements: None.
CutterSubtype¶
-
MillToolBuilder.
CutterSubtype
¶ Returns or sets the cutter subtypes
-------------------------------------
Getter Method
Signature
CutterSubtype()
Returns: Return type: NXOpen.CAM.MillToolBuilderCutterSubtypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutterSubtype(cutterSubtype)
Parameters: cutterSubtype ( NXOpen.CAM.MillToolBuilderCutterSubtypes
) –New in version NX5.0.0.
License requirements: None.
TlCor1RadBuilder¶
-
MillToolBuilder.
TlCor1RadBuilder
¶ Returns the Lower Radius builder (inheritable double)
-------------------------------------
Getter Method
Signature
TlCor1RadBuilder()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
TlCor2RadBuilder¶
-
MillToolBuilder.
TlCor2RadBuilder
¶ Returns the Upper Radius builder (inheritable double)
-------------------------------------
Getter Method
Signature
TlCor2RadBuilder()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
TlTipAngBuilder¶
-
MillToolBuilder.
TlTipAngBuilder
¶ Returns the Tip Angle builder (inheritable double)
-------------------------------------
Getter Method
Signature
TlTipAngBuilder()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
TlXcenCor1Builder¶
-
MillToolBuilder.
TlXcenCor1Builder
¶ Returns the X Center R1 builder (inheritable double)
-------------------------------------
Getter Method
Signature
TlXcenCor1Builder()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
TlXcenCor2Builder¶
-
MillToolBuilder.
TlXcenCor2Builder
¶ Returns the X Center R2 builder (inheritable double)
-------------------------------------
Getter Method
Signature
TlXcenCor2Builder()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
TlYcenCor1Builder¶
-
MillToolBuilder.
TlYcenCor1Builder
¶ Returns the Y Center R1 builder (inheritable double)
-------------------------------------
Getter Method
Signature
TlYcenCor1Builder()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
TlYcenCor2Builder¶
-
MillToolBuilder.
TlYcenCor2Builder
¶ Returns the Y Center R2 builder (inheritable double)
-------------------------------------
Getter Method
Signature
TlYcenCor2Builder()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
MillToolBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.