MillBoundaryGeomBuilder Class¶
-
class
NXOpen.CAM.
MillBoundaryGeomBuilder
¶ Bases:
NXOpen.CAM.FeatureGeomBuilder
Represents a MillBoundaryGeom Builder
To create a new instance of this class, use
NXOpen.CAM.NCGroupCollection.CreateMillBoundaryGeomBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BlankBoundary | Returns the blank boundary |
BlankOffsetBuilder | Returns the blank offset (inheritable double) |
CheckBoundary | Returns the check boundary |
CheckOffsetBuilder | Returns the check offset (inheritable double) |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndUdeSet | Returns the end ude set |
GeometryCiBuilder | Returns the geometry builder |
LayoutCiBuilder | Returns the save/layer layout builder |
OptimizationMethod | Returns or sets the optim method |
PartBoundary | Returns the part boundary |
PartMaterialBuilder | Returns or sets the part material |
PartOffsetBuilder | Returns the part offset (inheritable double) |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
TrimBoundary | Returns the trim boundary |
TrimOffsetBuilder | Returns the trim offset (inheritable double) |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetMaterial | Get part material @return |
GetMaterialData | Get material data |
GetObject | Returns the object currently being edited by this builder. |
SetMaterial | Set part material |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BlankBoundary¶
-
MillBoundaryGeomBuilder.
BlankBoundary
¶ Returns the blank boundary
-------------------------------------
Getter Method
Signature
BlankBoundary()
Returns: Return type: NXOpen.CAM.Boundary
New in version NX9.0.0.
License requirements: None.
CheckBoundary¶
-
MillBoundaryGeomBuilder.
CheckBoundary
¶ Returns the check boundary
-------------------------------------
Getter Method
Signature
CheckBoundary()
Returns: Return type: NXOpen.CAM.Boundary
New in version NX9.0.0.
License requirements: None.
PartBoundary¶
-
MillBoundaryGeomBuilder.
PartBoundary
¶ Returns the part boundary
-------------------------------------
Getter Method
Signature
PartBoundary()
Returns: Return type: NXOpen.CAM.Boundary
New in version NX9.0.0.
License requirements: None.
TrimBoundary¶
-
MillBoundaryGeomBuilder.
TrimBoundary
¶ Returns the trim boundary
-------------------------------------
Getter Method
Signature
TrimBoundary()
Returns: Return type: NXOpen.CAM.Boundary
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
MillBoundaryGeomBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.