LaserSlotCutout Class¶
-
class
NXOpen.CAM.
LaserSlotCutout
¶ Bases:
NXOpen.CAM.MoveBuilder
Represents a LaserSlotCutout
To create a new instance of this class, use
NXOpen.CAM.MoveCollection.CreateLaserSlotCutout
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CutDirection | Returns the Cut Direction |
CutoutDefinition | Returns the Cutout Definition |
FeedRate | Returns or sets the feed rate |
FeedType | Returns or sets the feed type |
FeedUnit | Returns or sets the feed unit |
HeadOrientation | Returns the Head Orientation |
MotionType | Returns or sets the motion type |
NumberOfUserParameters | Returns the number of user parameters |
PiercingPoint | Returns the Piercing Point |
ProtectedMove | Returns or sets the protected move status |
SubopLabel | Returns or sets the subop label |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetUserParameter | Returns the custom parameter with the given name. |
SetParent | Set parent |
SetSibling | Set sibling |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CutDirection¶
-
LaserSlotCutout.
CutDirection
¶ Returns the Cut Direction
-------------------------------------
Getter Method
Signature
CutDirection()
Returns: Return type: NXOpen.CAM.LaserCutDirection
New in version NX9.0.0.
License requirements: None.
CutoutDefinition¶
-
LaserSlotCutout.
CutoutDefinition
¶ Returns the Cutout Definition
-------------------------------------
Getter Method
Signature
CutoutDefinition()
Returns: Return type: NXOpen.CAM.LaserCutoutDefinition
New in version NX9.0.0.
License requirements: None.
HeadOrientation¶
-
LaserSlotCutout.
HeadOrientation
¶ Returns the Head Orientation
-------------------------------------
Getter Method
Signature
HeadOrientation()
Returns: Return type: NXOpen.CAM.LaserHeadOrientation
New in version NX9.0.0.
License requirements: None.
PiercingPoint¶
-
LaserSlotCutout.
PiercingPoint
¶ Returns the Piercing Point
-------------------------------------
Getter Method
Signature
PiercingPoint()
Returns: Return type: NXOpen.CAM.LaserPiercingPoint
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
LaserSlotCutout.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.