InspectionSensorMassEditBuilder Class¶
-
class
NXOpen.CAM.
InspectionSensorMassEditBuilder
¶ Bases:
NXOpen.Builder
Edit Multiple Subops Dialog builder
To create a new instance of this class, use
NXOpen.CAM.InspectionMoveCollection.CreateInspectionSensorMassEditBuilder
New in version NX7.5.3.
Properties¶
Property | Description |
---|---|
AngleA | Returns or sets the angle a |
AngleB | Returns or sets the angle b |
SensorName | Returns or sets the sensor name |
SensorStrategy | Returns or sets the sensor strategy |
Tag | Returns the Tag for this object. |
TipNumber | Returns or sets the tip |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
InspectionSensorMassEditBuilderSensorSelectModeType Enumeration | the sensor selection mode |
InspectionSensorMassEditBuilderSensorStrategyType Enumeration | the sensor strategy |
Property Detail¶
AngleA¶
-
InspectionSensorMassEditBuilder.
AngleA
¶ Returns or sets the angle a
-------------------------------------
Getter Method
Signature
AngleA()
Returns: Return type: float New in version NX7.5.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleA(angleA)
Parameters: angleA (float) – New in version NX7.5.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
AngleB¶
-
InspectionSensorMassEditBuilder.
AngleB
¶ Returns or sets the angle b
-------------------------------------
Getter Method
Signature
AngleB()
Returns: Return type: float New in version NX7.5.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleB(angleB)
Parameters: angleB (float) – New in version NX7.5.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SensorName¶
-
InspectionSensorMassEditBuilder.
SensorName
¶ Returns or sets the sensor name
-------------------------------------
Getter Method
Signature
SensorName()
Returns: Return type: str New in version NX7.5.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
SensorName(sensorName)
Parameters: sensorName (str) – New in version NX7.5.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SensorStrategy¶
-
InspectionSensorMassEditBuilder.
SensorStrategy
¶ Returns or sets the sensor strategy
-------------------------------------
Getter Method
Signature
SensorStrategy()
Returns: Return type: NXOpen.CAM.InspectionSensorMassEditBuilderSensorStrategyType
New in version NX7.5.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
SensorStrategy(sensorStrategy)
Parameters: sensorStrategy ( NXOpen.CAM.InspectionSensorMassEditBuilderSensorStrategyType
) –New in version NX7.5.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TipNumber¶
-
InspectionSensorMassEditBuilder.
TipNumber
¶ Returns or sets the tip
-------------------------------------
Getter Method
Signature
TipNumber()
Returns: Return type: int New in version NX7.5.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
TipNumber(tipNumber)
Parameters: tipNumber (int) – New in version NX7.5.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
Validate¶
-
InspectionSensorMassEditBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.