InspectionSensorMassEditBuilderSensorSelectModeType Enumeration¶
NXOpen.CAM.InspectionSensorMassEditBuilder.SensorSelectModeType is an alias for NXOpen.CAM.InspectionSensorMassEditBuilderSensorSelectModeType
-
class
NXOpen.CAM.
InspectionSensorMassEditBuilderSensorSelectModeType
¶ Bases:
object
the sensor selection mode
Enum Members
Enum Member Enum Member Description Automatic Choose sensor automaticallySpecifySensor Manually specify sensorSpecifyProbeAngles Manually specify probe anglesSpecifyProbeTip Manually specify probe tipSpecifyAnglesandTip Manually specify probe angles and probe tip-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-