InspectionProbeTrackingBuilder Class¶
-
class
NXOpen.CAM.
InspectionProbeTrackingBuilder
¶ Bases:
NXOpen.CAM.SolidTrackingBuilder
Represents a InspectionProbeTracking builder
To create a new instance of this class, use
NXOpen.CAM.InspectionTool.CreateInspectionProbeTrackingBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AxialPercent | Returns or sets the axial percentage |
Axis | Returns or sets the stem axis |
Location | Returns or sets the location |
StemTop | Returns or sets the stem top |
Tag | Returns the Tag for this object. |
TipType | Returns or sets the tip type |
TlAdjReg | Returns or sets the adjust register |
TlCutcomReg | Returns or sets the cutcom register |
TrackingName | Returns or sets the Tracking Point name value |
TrackingXOff | Returns or sets the XOff value |
TrackingYOff | Returns or sets the YOff value |
TrackingZOff | Returns or sets the ZOff value |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetLocationParameters | Set the trackpoint location and default parameters |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
InspectionProbeTrackingBuilderTipTypes Enumeration | the tip type |
Property Detail¶
AxialPercent¶
-
InspectionProbeTrackingBuilder.
AxialPercent
¶ Returns or sets the axial percentage
-------------------------------------
Getter Method
Signature
AxialPercent()
Returns: the axial percentage Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AxialPercent(pct)
Parameters: pct (float) – the axial percentage New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Axis¶
-
InspectionProbeTrackingBuilder.
Axis
¶ Returns or sets the stem axis
-------------------------------------
Getter Method
Signature
Axis()
Returns: the axis tag Return type: NXOpen.NXObject
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Axis(axis)
Parameters: axis ( NXOpen.NXObject
) – the axis tagNew in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StemTop¶
-
InspectionProbeTrackingBuilder.
StemTop
¶ Returns or sets the stem top
-------------------------------------
Getter Method
Signature
StemTop()
Returns: the stem_top tag Return type: NXOpen.NXObject
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StemTop(stemTop)
Parameters: stemTop ( NXOpen.NXObject
) – the stem_top tagNew in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TipType¶
-
InspectionProbeTrackingBuilder.
TipType
¶ Returns or sets the tip type
-------------------------------------
Getter Method
Signature
TipType()
Returns: Return type: NXOpen.CAM.InspectionProbeTrackingBuilderTipTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TipType(type)
Parameters: type ( NXOpen.CAM.InspectionProbeTrackingBuilderTipTypes
) –New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
SetLocationParameters¶
-
InspectionProbeTrackingBuilder.
SetLocationParameters
¶ Set the trackpoint location and default parameters
Signature
SetLocationParameters(tpLocation)
Parameters: tpLocation ( NXOpen.NXObject
) – the trackpoint geometryNew in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionProbeTrackingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.