SolidTrackingBuilder Class¶
-
class
NXOpen.CAM.
SolidTrackingBuilder
¶ Bases:
NXOpen.CAM.TrackpointBuilder
Represents a SolidTracking Builder
To create a new instance of this class, use
NXOpen.CAM.Tool.CreateSolidTrackingBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Location | Returns or sets the location |
Tag | Returns the Tag for this object. |
TlAdjReg | Returns or sets the adjust register |
TlCutcomReg | Returns or sets the cutcom register |
TrackingName | Returns or sets the Tracking Point name value |
TrackingXOff | Returns or sets the XOff value |
TrackingYOff | Returns or sets the YOff value |
TrackingZOff | Returns or sets the ZOff value |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Location¶
-
SolidTrackingBuilder.
Location
¶ Returns or sets the location
-------------------------------------
Getter Method
Signature
Location()
Returns: the tracking point Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Location(tpLocation)
Parameters: tpLocation ( NXOpen.NXObject
) – the tracking point tagNew in version NX5.0.0.
License requirements: None.
TrackingXOff¶
-
SolidTrackingBuilder.
TrackingXOff
¶ Returns or sets the XOff value
-------------------------------------
Getter Method
Signature
TrackingXOff()
Returns: the xoff value Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrackingXOff(xoffValue)
Parameters: xoffValue (float) – the xoff value New in version NX5.0.0.
License requirements: None.
TrackingYOff¶
-
SolidTrackingBuilder.
TrackingYOff
¶ Returns or sets the YOff value
-------------------------------------
Getter Method
Signature
TrackingYOff()
Returns: the yoff value Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrackingYOff(yoffValue)
Parameters: yoffValue (float) – the yoff value New in version NX5.0.0.
License requirements: None.
TrackingZOff¶
-
SolidTrackingBuilder.
TrackingZOff
¶ Returns or sets the ZOff value
-------------------------------------
Getter Method
Signature
TrackingZOff()
Returns: the zoff value Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrackingZOff(zoffValue)
Parameters: zoffValue (float) – the zoff value New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
SolidTrackingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.