GrooveToolBuilder Class¶
-
class
NXOpen.CAM.
GrooveToolBuilder
¶ Bases:
NXOpen.CAM.TurningToolBuilder
Represents a Groove tool builder
To create a new instance of this class, use
NXOpen.CAM.NCGroupCollection.CreateGrooveToolBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ChannelName | Returns or sets the channel’s name |
CutterExportBuilder | Returns the cutter export builder |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndUdeSet | Returns the end ude set |
HolderAngleBuilder | Returns the holder angle builder (inheritable double) |
HolderDescription | Returns or sets the holder description |
HolderGrooveHand | Returns or sets the holder groove hand |
HolderHand | Returns or sets the holder hand |
HolderInsertExtensionBuilder | Returns the holder insert extension builder (inheritable double) for groove tools |
HolderLengthBuilder | Returns the turn holder length builder (inheritable double) |
HolderLibraryReference | Returns or sets the holder libref |
HolderLock | Returns or sets the lock turn holder toggle |
HolderShankLineBuilder | Returns the turn holder shank line builder (inheritable double) |
HolderShankType | Returns or sets the turn holder shank type |
HolderShankWidthBuilder | Returns the turn holder shank width builder (inheritable double) |
HolderStyle | Returns or sets the holder style |
HolderUse | Returns or sets the use turn holder toggle |
HolderWidthBuilder | Returns the turn holder width builder (inheritable double) |
InsertLengthBuilder | Returns the insert length builder (inheritable double) |
InsertPosition | Returns or sets the insert position |
InsertShape | Returns or sets the insert shape |
InsertWidthBuilder | Returns the insert width builder (inheritable double) |
LeftAngleBuilder | Returns the left angle builder (inheritable double) |
LeftRadiusBuilder | Returns the left radius builder (inheritable double) |
LibraryParametersBuilder | Returns the Library Data Object |
ManageToolPartBuilder | Returns the manage tool part builder |
MaxDepthBuilder | Returns the max. |
MaxDepthToggle | Returns or sets the max. |
MaxFacingDiameterBuilder | Returns the max. |
MaxFacingDiameterToggle | Returns or sets the max. |
MaxToolReachBuilder | Returns the max. |
MaxToolReachToggle | Returns or sets the max. |
McsSpindleGroup | Returns or sets the MCS spindle group |
MinBoringDiameterBuilder | Returns the min. |
MinBoringDiameterToggle | Returns or sets the min. |
MinFacingDiameterBuilder | Returns the min. |
MinFacingDiameterToggle | Returns or sets the min. |
NoseRadiusBuilder | Returns the nose radius builder (inheritable double) |
NoseWidthBuilder | Returns the nose width builder (inheritable double) |
OptimizationMethod | Returns or sets the optim method |
OrientAngleBuilder | Returns the orient angle builder (inheritable double) |
RadiusBuilder | Returns the radius builder (inheritable double) |
RightAngleBuilder | Returns the right angle builder (inheritable double) |
RightRadiusBuilder | Returns the right radius builder (inheritable double) |
SideAngleBuilder | Returns the side angle builder (inheritable double) |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ThicknessBuilder | Returns the thickness builder (inheritable double) |
TipAngleBuilder | Returns the tip angle builder (inheritable double) |
TlCtlgNum | Returns or sets the Catalog Number |
TlDescription | Returns or sets the Cutter Description |
TlHolderNumberBuilder | Returns the Holder Number |
TlLibref | Returns or sets the Cutter Libref |
TlManualToolChange | Returns or sets the Manual Tool Change |
TlNumberBuilder | Returns the Tool Number |
TlText | Returns or sets the tool text |
TrackingBuilder | Returns the tracking point builder |
XMountBuilder | Returns the x mount builder (inheritable double) |
YMountBuilder | Returns the y mount builder (inheritable double) |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetMaterial | Get tool material @return |
GetMaterialData | Get material data |
GetObject | Returns the object currently being edited by this builder. |
SetMaterial | Set tool material |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
GrooveToolBuilderHolderGrooveHands Enumeration | The available holder groove hand options for groove tools |
GrooveToolBuilderHolderHands Enumeration | The available holder hand options for groove tools |
GrooveToolBuilderHolderStyles Enumeration | The available holder style options for groove tools |
GrooveToolBuilderInsertShapes Enumeration | The available insert shapes for groove tools |
Property Detail¶
HolderGrooveHand¶
-
GrooveToolBuilder.
HolderGrooveHand
¶ Returns or sets the holder groove hand
-------------------------------------
Getter Method
Signature
HolderGrooveHand()
Returns: Return type: NXOpen.CAM.GrooveToolBuilderHolderGrooveHands
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
HolderGrooveHand(holderHand)
Parameters: holderHand ( NXOpen.CAM.GrooveToolBuilderHolderGrooveHands
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
HolderHand¶
-
GrooveToolBuilder.
HolderHand
¶ Returns or sets the holder hand
-------------------------------------
Getter Method
Signature
HolderHand()
Returns: Return type: NXOpen.CAM.GrooveToolBuilderHolderHands
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HolderHand(holderHand)
Parameters: holderHand ( NXOpen.CAM.GrooveToolBuilderHolderHands
) –New in version NX5.0.0.
License requirements: None.
HolderInsertExtensionBuilder¶
-
GrooveToolBuilder.
HolderInsertExtensionBuilder
¶ Returns the holder insert extension builder (inheritable double) for groove tools
-------------------------------------
Getter Method
Signature
HolderInsertExtensionBuilder()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
HolderStyle¶
-
GrooveToolBuilder.
HolderStyle
¶ Returns or sets the holder style
-------------------------------------
Getter Method
Signature
HolderStyle()
Returns: Return type: NXOpen.CAM.GrooveToolBuilderHolderStyles
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HolderStyle(holderStyle)
Parameters: holderStyle ( NXOpen.CAM.GrooveToolBuilderHolderStyles
) –New in version NX5.0.0.
License requirements: None.
InsertShape¶
-
GrooveToolBuilder.
InsertShape
¶ Returns or sets the insert shape
-------------------------------------
Getter Method
Signature
InsertShape()
Returns: Return type: NXOpen.CAM.GrooveToolBuilderInsertShapes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InsertShape(insertShape)
Parameters: insertShape ( NXOpen.CAM.GrooveToolBuilderInsertShapes
) –New in version NX5.0.0.
License requirements: None.
LeftRadiusBuilder¶
-
GrooveToolBuilder.
LeftRadiusBuilder
¶ Returns the left radius builder (inheritable double)
-------------------------------------
Getter Method
Signature
LeftRadiusBuilder()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
RadiusBuilder¶
-
GrooveToolBuilder.
RadiusBuilder
¶ Returns the radius builder (inheritable double)
-------------------------------------
Getter Method
Signature
RadiusBuilder()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
RightRadiusBuilder¶
-
GrooveToolBuilder.
RightRadiusBuilder
¶ Returns the right radius builder (inheritable double)
-------------------------------------
Getter Method
Signature
RightRadiusBuilder()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
SideAngleBuilder¶
-
GrooveToolBuilder.
SideAngleBuilder
¶ Returns the side angle builder (inheritable double)
-------------------------------------
Getter Method
Signature
SideAngleBuilder()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
TipAngleBuilder¶
-
GrooveToolBuilder.
TipAngleBuilder
¶ Returns the tip angle builder (inheritable double)
-------------------------------------
Getter Method
Signature
TipAngleBuilder()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
GrooveToolBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.