DriveMode Class¶
-
class
NXOpen.CAM.
DriveMode
¶ Bases:
NXOpen.TaggedObject
Drive Mode Builder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
FloorOverlap | Returns the Floor Overlap Distance |
Mode | Returns or sets the Drive Mode Type |
ReferenceToolDiameter | Returns or sets the Reference Tool Diameter |
Tag | Returns the Tag for this object. |
WallOverlap | Returns the Wall Overlap Distance |
Methods¶
Enumerations¶
DriveModeType Enumeration | Available types for Drive Mode |
Property Detail¶
FloorOverlap¶
-
DriveMode.
FloorOverlap
¶ Returns the Floor Overlap Distance
-------------------------------------
Getter Method
Signature
FloorOverlap()
Returns: the Floor Overlap Distance Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
Mode¶
-
DriveMode.
Mode
¶ Returns or sets the Drive Mode Type
-------------------------------------
Getter Method
Signature
Mode()
Returns: the Drive Mode Return type: NXOpen.CAM.DriveModeType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Mode(type)
Parameters: type ( NXOpen.CAM.DriveModeType
) – the Drive ModeNew in version NX7.5.0.
License requirements: None.
ReferenceToolDiameter¶
-
DriveMode.
ReferenceToolDiameter
¶ Returns or sets the Reference Tool Diameter
-------------------------------------
Getter Method
Signature
ReferenceToolDiameter()
Returns: the Reference Tool Diameter Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceToolDiameter(toolDia)
Parameters: toolDia (float) – the Reference Tool Diameter New in version NX7.5.0.
License requirements: None.
WallOverlap¶
-
DriveMode.
WallOverlap
¶ Returns the Wall Overlap Distance
-------------------------------------
Getter Method
Signature
WallOverlap()
Returns: the Wall Overlap Distance Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.