DriveModeType Enumeration¶
NXOpen.CAM.DriveMode.Type is an alias for NXOpen.CAM.DriveModeType
-
class
NXOpen.CAM.
DriveModeType
¶ Bases:
object
Available types for Drive Mode
New in version NX7.5.0.
Enum Members
Enum Member Enum Member Description LowerBlendEdge Lower Blend Edge ReferenceTool Reference Tool -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-