DrillGeomBuilder Class¶
-
class
NXOpen.CAM.
DrillGeomBuilder
¶ Bases:
NXOpen.CAM.FeatureGeomBuilder
Represents a DrillGeom Builder
To create a new instance of this class, use
NXOpen.CAM.NCGroupCollection.CreateDrillGeomBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BlankOffsetBuilder | Returns the blank offset (inheritable double) |
BottomSurface | Returns the bottom surface builder |
CheckOffsetBuilder | Returns the check offset (inheritable double) |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndUdeSet | Returns the end ude set |
GeometryCiBuilder | Returns the geometry builder |
LayoutCiBuilder | Returns the save/layer layout builder |
OptimizationMethod | Returns or sets the optim method |
PartMaterialBuilder | Returns or sets the part material |
PartOffsetBuilder | Returns the part offset (inheritable double) |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolAxisAsArcAxis | Returns or sets the Tool Axis as Arc Axis |
ToolAxisVector | Returns or sets the Tool Axis vector |
TopSurface | Returns the top surface builder |
TrimOffsetBuilder | Returns the trim offset (inheritable double) |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetMaterial | Get part material @return |
GetMaterialData | Get material data |
GetObject | Returns the object currently being edited by this builder. |
GetToolAxisType | Returns the Tool Axis type @return the integer value |
SetMaterial | Set part material |
SetToolAxisType | Sets the Tool Axis type |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BottomSurface¶
-
DrillGeomBuilder.
BottomSurface
¶ Returns the bottom surface builder
-------------------------------------
Getter Method
Signature
BottomSurface()
Returns: The bottom surface builder Return type: NXOpen.CAM.DrillSurfaceBuilder
New in version NX7.5.0.
License requirements: None.
ToolAxisAsArcAxis¶
-
DrillGeomBuilder.
ToolAxisAsArcAxis
¶ Returns or sets the Tool Axis as Arc Axis
-------------------------------------
Getter Method
Signature
ToolAxisAsArcAxis()
Returns: the current toggle value Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
ToolAxisAsArcAxis(toggleValue)
Parameters: toggleValue (int) – the new toggle value New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
ToolAxisVector¶
-
DrillGeomBuilder.
ToolAxisVector
¶ Returns or sets the Tool Axis vector
-------------------------------------
Getter Method
Signature
ToolAxisVector()
Returns: the vector tag Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
ToolAxisVector(vector)
Parameters: vector ( NXOpen.NXObject
) – the vector tagNew in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
TopSurface¶
-
DrillGeomBuilder.
TopSurface
¶ Returns the top surface builder
-------------------------------------
Getter Method
Signature
TopSurface()
Returns: The top surface builder Return type: NXOpen.CAM.DrillSurfaceBuilder
New in version NX7.5.0.
License requirements: None.
Method Detail¶
GetToolAxisType¶
-
DrillGeomBuilder.
GetToolAxisType
¶ Returns the Tool Axis type
Signature
GetToolAxisType()
Returns: the integer value Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
SetToolAxisType¶
-
DrillGeomBuilder.
SetToolAxisType
¶ Sets the Tool Axis type
Signature
SetToolAxisType(value)
Parameters: value (int) – the integer value New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
Validate¶
-
DrillGeomBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.