ChipControl Class¶
-
class
NXOpen.CAM.
ChipControl
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.ChipControl
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ConstantIncrement | Returns the Constant Increment |
DepartureDistance | Returns the Departure Distance |
FirstPlungeOnly | Returns or sets the First Plunge Only |
Tag | Returns the Tag for this object. |
Type | Returns or sets the chip control type |
VariableIncrement | Returns the Variable Increment |
Methods¶
Enumerations¶
ChipControlTypes Enumeration | the control mode options |
Property Detail¶
ConstantIncrement¶
-
ChipControl.
ConstantIncrement
¶ Returns the Constant Increment
-------------------------------------
Getter Method
Signature
ConstantIncrement()
Returns: the Constant Increment Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
DepartureDistance¶
-
ChipControl.
DepartureDistance
¶ Returns the Departure Distance
-------------------------------------
Getter Method
Signature
DepartureDistance()
Returns: the Departure Distance Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
FirstPlungeOnly¶
-
ChipControl.
FirstPlungeOnly
¶ Returns or sets the First Plunge Only
-------------------------------------
Getter Method
Signature
FirstPlungeOnly()
Returns: the First Plunge Only Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstPlungeOnly(firstPlungeOnly)
Parameters: firstPlungeOnly (bool) – the First Plunge Only New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Type¶
-
ChipControl.
Type
¶ Returns or sets the chip control type
-------------------------------------
Getter Method
Signature
Type()
Returns: the chip control type Return type: NXOpen.CAM.ChipControlTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(chipControlMode)
Parameters: chipControlMode ( NXOpen.CAM.ChipControlTypes
) – the chip control typeNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
VariableIncrement¶
-
ChipControl.
VariableIncrement
¶ Returns the Variable Increment
-------------------------------------
Getter Method
Signature
VariableIncrement()
Returns: the Variable Increment Return type: NXOpen.CAM.TurnRoughVariableIncrementBuilder
New in version NX6.0.0.
License requirements: None.