ChipControlTypes Enumeration¶
NXOpen.CAM.ChipControl.Types is an alias for NXOpen.CAM.ChipControlTypes
-
class
NXOpen.CAM.
ChipControlTypes
¶ Bases:
object
the control mode options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description None Chip control mode: NoneConstBreak Chip control mode: Constant BreakVarBreak Chip control mode: Variable BreakConstClear Chip control mode: Constant ClearVarClear Chip control mode: Variable Clear-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-