StrengthResultsEvaluationSettingBuilder Class¶
-
class
NXOpen.CAE.ResponseSimulation.
StrengthResultsEvaluationSettingBuilder
¶ Bases:
NXOpen.CAE.ResponseSimulation.DynamicResultEvaluationSettingBuilder
This is a manager to the
NXOpen.CAE.ResponseSimulation.StrengthResultsEvaluationSetting
class.Object of type
NXOpen.CAE.ResponseSimulation.StrengthResultsEvaluationSetting
can be created and edited only through this classTo create a new instance of this class, use
NXOpen.CAE.ResponseSimulation.EvaluationSettingManager.CreateStrengthResultsEvaluationSettingBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CombinationOptionsBuilder | Returns the setting of combination evaluation |
DataLocation | Returns the setting of combination evaluation |
MaterialDefinitionType | Returns or sets the definition method of material |
MaterialOverrideOption | Returns or sets the choice of override material property or not. |
MaterialSafetyFactor | Returns or sets the customized material safety factor |
StandardDeviation | Returns or sets the customized standard deviation for random event |
StressCriteriaType | Returns or sets the stress criteria type |
StressOptionType | Returns or sets the stress option type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDescriptionString | Returns the description. |
GetDestinationElements | Returns the destination elements @return |
GetObject | Returns the object currently being edited by this builder. |
SetDescriptionString | Sets the description |
SetDestinationElements | Sets the destination elements |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CombinationOptionsBuilder¶
-
StrengthResultsEvaluationSettingBuilder.
CombinationOptionsBuilder
¶ Returns the setting of combination evaluation
-------------------------------------
Getter Method
Signature
CombinationOptionsBuilder()
Returns: Return type: NXOpen.CAE.ResponseSimulation.CombinationEvaluationOptions
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
DataLocation¶
-
StrengthResultsEvaluationSettingBuilder.
DataLocation
¶ Returns the setting of combination evaluation
-------------------------------------
Getter Method
Signature
DataLocation()
Returns: Return type: NXOpen.CAE.ResponseSimulation.DataLocation
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
MaterialDefinitionType¶
-
StrengthResultsEvaluationSettingBuilder.
MaterialDefinitionType
¶ Returns or sets the definition method of material
-------------------------------------
Getter Method
Signature
MaterialDefinitionType()
Returns: Return type: NXOpen.CAE.ResponseSimulation.StrengthStressMaterialDefinitionMethod
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
MaterialDefinitionType(materialProperty)
Parameters: materialProperty ( NXOpen.CAE.ResponseSimulation.StrengthStressMaterialDefinitionMethod
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
MaterialOverrideOption¶
-
StrengthResultsEvaluationSettingBuilder.
MaterialOverrideOption
¶ Returns or sets the choice of override material property or not.
If false, the material safty factor will be read from destination element selected, else a customized value will be used
-------------------------------------
Getter Method
Signature
MaterialOverrideOption()
Returns: NRC_Double_Sum Time Duration Return type: bool New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
MaterialOverrideOption(overrideMaterialProperty)
Parameters: overrideMaterialProperty (bool) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
MaterialSafetyFactor¶
-
StrengthResultsEvaluationSettingBuilder.
MaterialSafetyFactor
¶ Returns or sets the customized material safety factor
-------------------------------------
Getter Method
Signature
MaterialSafetyFactor()
Returns: NRC_Double_Sum Time Duration Return type: float New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
MaterialSafetyFactor(safetyFactor)
Parameters: safetyFactor (float) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
StandardDeviation¶
-
StrengthResultsEvaluationSettingBuilder.
StandardDeviation
¶ Returns or sets the customized standard deviation for random event
-------------------------------------
Getter Method
Signature
StandardDeviation()
Returns: Random Event Standard Deviation Return type: float New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
StandardDeviation(standardDeviation)
Parameters: standardDeviation (float) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
StressCriteriaType¶
-
StrengthResultsEvaluationSettingBuilder.
StressCriteriaType
¶ Returns or sets the stress criteria type
-------------------------------------
Getter Method
Signature
StressCriteriaType()
Returns: Return type: NXOpen.CAE.ResponseSimulation.StrengthStressCriteria
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
StressCriteriaType(stressCriteria)
Parameters: stressCriteria ( NXOpen.CAE.ResponseSimulation.StrengthStressCriteria
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
StressOptionType¶
-
StrengthResultsEvaluationSettingBuilder.
StressOptionType
¶ Returns or sets the stress option type
-------------------------------------
Getter Method
Signature
StressOptionType()
Returns: Return type: NXOpen.CAE.ResponseSimulation.StrengthStressOption
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
StressOptionType(stressOption)
Parameters: stressOption ( NXOpen.CAE.ResponseSimulation.StrengthStressOption
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Method Detail¶
GetDestinationElements¶
-
StrengthResultsEvaluationSettingBuilder.
GetDestinationElements
¶ Returns the destination elements
Signature
GetDestinationElements()
Returns: Return type: list of NXOpen.CAE.FEElement
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SetDestinationElements¶
-
StrengthResultsEvaluationSettingBuilder.
SetDestinationElements
¶ Sets the destination elements
Signature
SetDestinationElements(destinationElement)
Parameters: destinationElement (list of NXOpen.CAE.FEElement
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Validate¶
-
StrengthResultsEvaluationSettingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.