DynamicResultEvaluationSettingBuilder Class¶
-
class
NXOpen.CAE.ResponseSimulation.
DynamicResultEvaluationSettingBuilder
¶ Bases:
NXOpen.Builder
Represents the abstract builder class of evaluation setting for all dynamic results evaluations.
This is an abstract class, and cannot be created.
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDescriptionString | Returns the description. |
GetObject | Returns the object currently being edited by this builder. |
SetDescriptionString | Sets the description |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
GetDescriptionString¶
-
DynamicResultEvaluationSettingBuilder.
GetDescriptionString
¶ Returns the description.
Signature
GetDescriptionString()
Returns: Return type: list of str New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SetDescriptionString¶
-
DynamicResultEvaluationSettingBuilder.
SetDescriptionString
¶ Sets the description
Signature
SetDescriptionString(description)
Parameters: description (list of str) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Validate¶
-
DynamicResultEvaluationSettingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.