SensorBuilder Class¶
-
class
NXOpen.CAE.ResponseSimulation.
SensorBuilder
¶ Bases:
NXOpen.CAE.ResponseSimulation.BaseBuilder
Represents a
NXOpen.CAE.ResponseSimulation.SensorBuilder
To create a new instance of this class, use
NXOpen.CAE.ResponseSimulation.SensorCollection.CreateSensorBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ObjectLabel | Returns the object label |
ReverseNormalDirection | Returns or sets the option for reverse the normal direction. |
SensorCoordinateType | Returns or sets the sensor’s coordinate type |
SensorDirectionX | Returns or sets the setting for x direction compontent of sensor. |
SensorDirectionY | Returns or sets the setting for y direction compontent of sensor. |
SensorDirectionZ | Returns or sets the setting for z direction compontent of sensor. |
SensorResultType | Returns or sets the sensor’s result type |
SensorRotationX | Returns or sets the setting for x rotation compontent of sensor. |
SensorRotationY | Returns or sets the setting for y rotation compontent of sensor. |
SensorRotationZ | Returns or sets the setting for z rotation compontent of sensor. |
SensorType | Returns or sets the sensor’s type |
SensorVector | Returns or sets the user defined direction. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetSelectedNodes | Returns the destination nodes @return |
SetSelectedNodes | Sets the destination nodes |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ReverseNormalDirection¶
-
SensorBuilder.
ReverseNormalDirection
¶ Returns or sets the option for reverse the normal direction.
Only available when the sensor type is
CAE.ResponseSimulationSensorType.Normal
-------------------------------------
Getter Method
Signature
ReverseNormalDirection()
Returns: Return type: bool New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ReverseNormalDirection(normalDirection)
Parameters: normalDirection (bool) – New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SensorCoordinateType¶
-
SensorBuilder.
SensorCoordinateType
¶ Returns or sets the sensor’s coordinate type
-------------------------------------
Getter Method
Signature
SensorCoordinateType()
Returns: Return type: NXOpen.CAE.ResponseSimulation.SensorCoordinateType
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
SensorCoordinateType(coordinateType)
Parameters: coordinateType ( NXOpen.CAE.ResponseSimulation.SensorCoordinateType
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SensorDirectionX¶
-
SensorBuilder.
SensorDirectionX
¶ Returns or sets the setting for x direction compontent of sensor.
If true, the response on direction x will be calculated. Only available when the sensor type is
CAE.ResponseSimulationSensorType.Component
-------------------------------------
Getter Method
Signature
SensorDirectionX()
Returns: Return type: bool New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
SensorDirectionX(directionX)
Parameters: directionX (bool) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SensorDirectionY¶
-
SensorBuilder.
SensorDirectionY
¶ Returns or sets the setting for y direction compontent of sensor.
If true, the response on direction y will be calculated. Only available when the sensor type is
CAE.ResponseSimulationSensorType.Component
-------------------------------------
Getter Method
Signature
SensorDirectionY()
Returns: Return type: bool New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
SensorDirectionY(directionY)
Parameters: directionY (bool) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SensorDirectionZ¶
-
SensorBuilder.
SensorDirectionZ
¶ Returns or sets the setting for z direction compontent of sensor.
If true, the response on direction z will be calculated. Only available when the sensor type is
CAE.ResponseSimulationSensorType.Component
-------------------------------------
Getter Method
Signature
SensorDirectionZ()
Returns: Return type: bool New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
SensorDirectionZ(directionZ)
Parameters: directionZ (bool) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SensorResultType¶
-
SensorBuilder.
SensorResultType
¶ Returns or sets the sensor’s result type
-------------------------------------
Getter Method
Signature
SensorResultType()
Returns: Return type: NXOpen.CAE.ResponseSimulation.SensorResultType
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
SensorResultType(resultType)
Parameters: resultType ( NXOpen.CAE.ResponseSimulation.SensorResultType
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SensorRotationX¶
-
SensorBuilder.
SensorRotationX
¶ Returns or sets the setting for x rotation compontent of sensor.
If true, the response on rotation x will be calculated. Only available when the sensor type is
CAE.ResponseSimulationSensorType.Component
-------------------------------------
Getter Method
Signature
SensorRotationX()
Returns: Return type: bool New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
SensorRotationX(rotationX)
Parameters: rotationX (bool) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SensorRotationY¶
-
SensorBuilder.
SensorRotationY
¶ Returns or sets the setting for y rotation compontent of sensor.
If true, the response on rotation y will be calculated. Only available when the sensor type is
CAE.ResponseSimulationSensorType.Component
-------------------------------------
Getter Method
Signature
SensorRotationY()
Returns: Return type: bool New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
SensorRotationY(rotationY)
Parameters: rotationY (bool) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SensorRotationZ¶
-
SensorBuilder.
SensorRotationZ
¶ Returns or sets the setting for z rotation compontent of sensor.
If true, the response on rotation z will be calculated. Only available when the sensor type is
CAE.ResponseSimulationSensorType.Component
-------------------------------------
Getter Method
Signature
SensorRotationZ()
Returns: Return type: bool New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
SensorRotationZ(rotationZ)
Parameters: rotationZ (bool) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SensorType¶
-
SensorBuilder.
SensorType
¶ Returns or sets the sensor’s type
-------------------------------------
Getter Method
Signature
SensorType()
Returns: Return type: NXOpen.CAE.ResponseSimulation.SensorType
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
SensorType(sensorType)
Parameters: sensorType ( NXOpen.CAE.ResponseSimulation.SensorType
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SensorVector¶
-
SensorBuilder.
SensorVector
¶ Returns or sets the user defined direction.
Only available when the sensor type is
CAE.ResponseSimulationSensorType.Direction
-------------------------------------
Getter Method
Signature
SensorVector()
Returns: Return type: NXOpen.Direction
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
SensorVector(sensorVector)
Parameters: sensorVector ( NXOpen.Direction
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Method Detail¶
GetSelectedNodes¶
-
SensorBuilder.
GetSelectedNodes
¶ Returns the destination nodes
Signature
GetSelectedNodes()
Returns: Return type: list of NXOpen.CAE.FENode
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SetSelectedNodes¶
-
SensorBuilder.
SetSelectedNodes
¶ Sets the destination nodes
Signature
SetSelectedNodes(destinationNodes)
Parameters: destinationNodes (list of NXOpen.CAE.FENode
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Validate¶
-
SensorBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.