DAOConstraintBuilder Class¶
-
class
NXOpen.CAE.Optimization.
DAOConstraintBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.Optimization.DAOConstraintBuilder
.To create a new instance of this class, use
NXOpen.CAE.Optimization.DAOSolutionCollection.CreateConstraintBuilder
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
CategoryType | Returns or sets the category type |
GeometryType | Returns or sets the geometry type |
LimitType | Returns or sets the limit type |
LimitUnit | Returns or sets the limit unit |
LimitValue | Returns or sets the limit value |
LoadCase | Returns or sets the frequency load case index |
ModeNumber | Returns or sets the frequency mode number |
Response | Returns or sets the constraint response |
ResultMeasure | Returns or sets the result measure |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetGeometry | Gets the target geometry @return Target geometry |
GetObject | Returns the object currently being edited by this builder. |
SetGeometry | Sets the target geometry |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CategoryType¶
-
DAOConstraintBuilder.
CategoryType
¶ Returns or sets the category type
-------------------------------------
Getter Method
Signature
CategoryType()
Returns: Category type Return type: NXOpen.CAE.Optimization.Category
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CategoryType(categoryType)
Parameters: categoryType ( NXOpen.CAE.Optimization.Category
) – Category typeNew in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GeometryType¶
-
DAOConstraintBuilder.
GeometryType
¶ Returns or sets the geometry type
-------------------------------------
Getter Method
Signature
GeometryType()
Returns: Geometry type Return type: NXOpen.CAE.Optimization.Geometry
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GeometryType(geometryType)
Parameters: geometryType ( NXOpen.CAE.Optimization.Geometry
) – Geometry typeNew in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
LimitType¶
-
DAOConstraintBuilder.
LimitType
¶ Returns or sets the limit type
-------------------------------------
Getter Method
Signature
LimitType()
Returns: Limit type Return type: NXOpen.CAE.Optimization.Limit
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitType(limitType)
Parameters: limitType ( NXOpen.CAE.Optimization.Limit
) – Limit typeNew in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
LimitUnit¶
-
DAOConstraintBuilder.
LimitUnit
¶ Returns or sets the limit unit
-------------------------------------
Getter Method
Signature
LimitUnit()
Returns: Limit unit Return type: NXOpen.Unit
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitUnit(targetUnit)
Parameters: targetUnit ( NXOpen.Unit
) – Limit unitNew in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
LimitValue¶
-
DAOConstraintBuilder.
LimitValue
¶ Returns or sets the limit value
-------------------------------------
Getter Method
Signature
LimitValue()
Returns: Limit value Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitValue(limitValue)
Parameters: limitValue (float) – Limit value New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
LoadCase¶
-
DAOConstraintBuilder.
LoadCase
¶ Returns or sets the frequency load case index
-------------------------------------
Getter Method
Signature
LoadCase()
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LoadCase(loadcase)
Parameters: loadcase (int) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ModeNumber¶
-
DAOConstraintBuilder.
ModeNumber
¶ Returns or sets the frequency mode number
-------------------------------------
Getter Method
Signature
ModeNumber()
Returns: Mode number Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ModeNumber(modeNumber)
Parameters: modeNumber (int) – Mode number New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Response¶
-
DAOConstraintBuilder.
Response
¶ Returns or sets the constraint response
-------------------------------------
Getter Method
Signature
Response()
Returns: Constraint response Return type: NXOpen.CAE.Optimization.Response
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Response(constraintResponse)
Parameters: constraintResponse ( NXOpen.CAE.Optimization.Response
) – Constraint responseNew in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ResultMeasure¶
-
DAOConstraintBuilder.
ResultMeasure
¶ Returns or sets the result measure
-------------------------------------
Getter Method
Signature
ResultMeasure()
Returns: Return type: NXOpen.CAE.ResultMeasure
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ResultMeasure(resMeas)
Parameters: resMeas ( NXOpen.CAE.ResultMeasure
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
GetGeometry¶
-
DAOConstraintBuilder.
GetGeometry
¶ Gets the target geometry
Signature
GetGeometry()
Returns: Target geometry Return type: list of NXOpen.DisplayableObject
New in version NX8.0.0.
License requirements: None.
SetGeometry¶
-
DAOConstraintBuilder.
SetGeometry
¶ Sets the target geometry
Signature
SetGeometry(geometry)
Parameters: geometry (list of NXOpen.DisplayableObject
) – Target geometryNew in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Validate¶
-
DAOConstraintBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.