RelinkerBuilder Class¶
-
class
NXOpen.Assemblies.
RelinkerBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Assemblies.RelinkerBuilder
To create a new instance of this class, use
NXOpen.Assemblies.RelinkerCollection.CreateBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BreakInterpartExpression | Returns or sets the option to break interpart expression. |
BreakWaveLink | Returns or sets the option to break WAVE links. |
FaceCurveDirectionAdjustment | Returns or sets the option to adjust face or curve direction. |
IncludeNonBrokenWaveLinks | Returns or sets the option to include non-broken WAVE links or not. |
IncludeSuppressedComponents | Returns or sets the option to include suppressed components as source candidates or not. |
RelinkCategory | Returns or sets the relink category either wave geometry or interpart expression. |
RelinkOption | Returns or sets the link option. |
RelinkType | Returns or sets the current link type. |
SearchingDestinationObject | Returns or sets the searching destination object string. |
SearchingSourceObject | Returns or sets the searching source object string. |
SearchingSourcePart | Returns or sets the searching source part string. |
SearchingSourcePartAttribute | Returns or sets the searching source part attribute string. |
SelectComponent | Returns a list of the selected component as relink target scope. |
SelectComponentSource | Returns a list of the selected component as relink source scope. |
SourceScope | Returns or sets the current source scope. |
Tag | Returns the Tag for this object. |
TargetScope | Returns or sets the current target scope. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
ExecuteRelink | Relink with new source, for WAVE links, interpart explression or both. |
ExportToInformationWindow | List all link information to the list window. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetExpressionSourceCount | Gets the total count of multiple candidate sources to re-parent the inter part expression. |
GetObject | Returns the object currently being edited by this builder. |
RelinkInterpartExpression | Relinks the inter part expression using the specific expression from the specific part in case of multiple expression sources. |
RelinkWaveFeature | Relinks the wave feature using the specific geometry source from the specific part in case of multiple geometry sources. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateSession | Updates the session. |
UpdateSessionWithBreakDelayed | Updates the session without immediately breaking wave links or inter part expressions. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ViewFeatureFailure | Views the feature failure information. |
Enumerations¶
RelinkerBuilderLinkCategory Enumeration | Represents the link category of Relinker, either geometry WAVE link or interpart expression. |
RelinkerBuilderLinkOption Enumeration | Represents the relink option. |
RelinkerBuilderLinkScope Enumeration | Represents the relink scope type of Relinker. |
RelinkerBuilderLinkType Enumeration | Represents the link type option when browsing current available links. |
Property Detail¶
BreakInterpartExpression¶
-
RelinkerBuilder.
BreakInterpartExpression
¶ Returns or sets the option to break interpart expression.
If it’s true, relinker will break interpart expression after relinking. If it’s false, relinker will not break interpart expression.
-------------------------------------
Getter Method
Signature
BreakInterpartExpression()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BreakInterpartExpression(breakInterPartExpression)
Parameters: breakInterPartExpression (bool) – New in version NX5.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
BreakWaveLink¶
-
RelinkerBuilder.
BreakWaveLink
¶ Returns or sets the option to break WAVE links.
If it’s true, relinker will break WAVE links after relinking. If it’s false, relinker will not break WAVE links.
-------------------------------------
Getter Method
Signature
BreakWaveLink()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BreakWaveLink(breakWave)
Parameters: breakWave (bool) – New in version NX5.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
FaceCurveDirectionAdjustment¶
-
RelinkerBuilder.
FaceCurveDirectionAdjustment
¶ Returns or sets the option to adjust face or curve direction.
If it’s true, relinker will check the linked curve direction or face normal and either keep or automatically flip the direction of new source while relinking.
-------------------------------------
Getter Method
Signature
FaceCurveDirectionAdjustment()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FaceCurveDirectionAdjustment(adjustDir)
Parameters: adjustDir (bool) – New in version NX5.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
IncludeNonBrokenWaveLinks¶
-
RelinkerBuilder.
IncludeNonBrokenWaveLinks
¶ Returns or sets the option to include non-broken WAVE links or not.
If it’s true, relinker will include non-broken WAVE links. If it’s false, non-broken WAVE links will not be included while relinking. The default behavior in the relinker is not to include non-broken WAVE links.
-------------------------------------
Getter Method
Signature
IncludeNonBrokenWaveLinks()
Returns: Return type: bool New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
IncludeNonBrokenWaveLinks(includeNonBrokenWaveLinks)
Parameters: includeNonBrokenWaveLinks (bool) – New in version NX5.0.2.
License requirements: wave (“WAVE FUNCTIONALITY”)
IncludeSuppressedComponents¶
-
RelinkerBuilder.
IncludeSuppressedComponents
¶ Returns or sets the option to include suppressed components as source candidates or not.
If it’s true, relinker will include suppressed components as source candidates. If it’s false, suppressed components will not be included as source candidates while relinking. The default behavior in the relinker is not to include suppressed components.
-------------------------------------
Getter Method
Signature
IncludeSuppressedComponents()
Returns: Return type: bool New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
IncludeSuppressedComponents(includeSuppressedComponents)
Parameters: includeSuppressedComponents (bool) – New in version NX5.0.2.
License requirements: wave (“WAVE FUNCTIONALITY”)
RelinkCategory¶
-
RelinkerBuilder.
RelinkCategory
¶ Returns or sets the relink category either wave geometry or interpart expression.
-------------------------------------
Getter Method
Signature
RelinkCategory()
Returns: Return type: NXOpen.Assemblies.RelinkerBuilderLinkCategory
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RelinkCategory(linkCategory)
Parameters: linkCategory ( NXOpen.Assemblies.RelinkerBuilderLinkCategory
) –New in version NX5.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
RelinkOption¶
-
RelinkerBuilder.
RelinkOption
¶ Returns or sets the link option.
Relinker will check this option to relink WAVE, interpart expression or both
-------------------------------------
Getter Method
Signature
RelinkOption()
Returns: Return type: NXOpen.Assemblies.RelinkerBuilderLinkOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RelinkOption(linkOption)
Parameters: linkOption ( NXOpen.Assemblies.RelinkerBuilderLinkOption
) –New in version NX5.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
RelinkType¶
-
RelinkerBuilder.
RelinkType
¶ Returns or sets the current link type.
-------------------------------------
Getter Method
Signature
RelinkType()
Returns: Return type: NXOpen.Assemblies.RelinkerBuilderLinkType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RelinkType(linkType)
Parameters: linkType ( NXOpen.Assemblies.RelinkerBuilderLinkType
) –New in version NX5.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
SearchingDestinationObject¶
-
RelinkerBuilder.
SearchingDestinationObject
¶ Returns or sets the searching destination object string.
Used to specify the wildcard string to search the destination objects when cycling object by name. When cycling destination objects, relink scope will be used as the searching scope.
-------------------------------------
Getter Method
Signature
SearchingDestinationObject()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SearchingDestinationObject(destinationObjectStr)
Parameters: destinationObjectStr (str) – New in version NX5.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
SearchingSourceObject¶
-
RelinkerBuilder.
SearchingSourceObject
¶ Returns or sets the searching source object string.
Used to specify the wildcard string to search the source objects when cycling object by name. When cycling source objects, source parts will define the searching scope.
-------------------------------------
Getter Method
Signature
SearchingSourceObject()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SearchingSourceObject(sourceObjectStr)
Parameters: sourceObjectStr (str) – New in version NX5.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
SearchingSourcePart¶
-
RelinkerBuilder.
SearchingSourcePart
¶ Returns or sets the searching source part string.
Used to specify the wildcard string to search source parts by file names. Source parts define the scope of searching source objects.
-------------------------------------
Getter Method
Signature
SearchingSourcePart()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SearchingSourcePart(sourcePartStr)
Parameters: sourcePartStr (str) – New in version NX5.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
SearchingSourcePartAttribute¶
-
RelinkerBuilder.
SearchingSourcePartAttribute
¶ Returns or sets the searching source part attribute string.
Used to specify the wildcard string to search source parts by part attribute predefined in source part. This criterial will furtherly narrow down the source part scope to avoid multiple source found.
-------------------------------------
Getter Method
Signature
SearchingSourcePartAttribute()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SearchingSourcePartAttribute(sourcePartAttribute)
Parameters: sourcePartAttribute (str) – New in version NX5.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
SelectComponent¶
-
RelinkerBuilder.
SelectComponent
¶ Returns a list of the selected component as relink target scope.
-------------------------------------
Getter Method
Signature
SelectComponent()
Returns: Return type: NXOpen.Assemblies.SelectComponentList
New in version NX5.0.0.
License requirements: None.
SelectComponentSource¶
-
RelinkerBuilder.
SelectComponentSource
¶ Returns a list of the selected component as relink source scope.
-------------------------------------
Getter Method
Signature
SelectComponentSource()
Returns: Return type: NXOpen.Assemblies.SelectComponentList
New in version NX6.0.2.
License requirements: None.
SourceScope¶
-
RelinkerBuilder.
SourceScope
¶ Returns or sets the current source scope.
-------------------------------------
Getter Method
Signature
SourceScope()
Returns: Return type: NXOpen.Assemblies.RelinkerBuilderLinkScope
New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
SourceScope(sourceScope)
Parameters: sourceScope ( NXOpen.Assemblies.RelinkerBuilderLinkScope
) –New in version NX5.0.2.
License requirements: wave (“WAVE FUNCTIONALITY”)
TargetScope¶
-
RelinkerBuilder.
TargetScope
¶ Returns or sets the current target scope.
-------------------------------------
Getter Method
Signature
TargetScope()
Returns: Return type: NXOpen.Assemblies.RelinkerBuilderLinkScope
New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetScope(targetScope)
Parameters: targetScope ( NXOpen.Assemblies.RelinkerBuilderLinkScope
) –New in version NX5.0.2.
License requirements: wave (“WAVE FUNCTIONALITY”)
Method Detail¶
ExecuteRelink¶
-
RelinkerBuilder.
ExecuteRelink
¶ Relink with new source, for WAVE links, interpart explression or both.
Signature
ExecuteRelink()
New in version NX5.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
ExportToInformationWindow¶
-
RelinkerBuilder.
ExportToInformationWindow
¶ List all link information to the list window.
Signature
ExportToInformationWindow()
New in version NX5.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
GetExpressionSourceCount¶
-
RelinkerBuilder.
GetExpressionSourceCount
¶ Gets the total count of multiple candidate sources to re-parent the inter part expression.
Signature
GetExpressionSourceCount(partID, expID, sourceID)
Parameters: - partID (
NXOpen.Part
) – - expID (
NXOpen.Expression
) – - sourceID (
NXOpen.Expression
) –
Returns: Return type: int
New in version NX7.5.5.
License requirements: wave (“WAVE FUNCTIONALITY”)
- partID (
RelinkInterpartExpression¶
-
RelinkerBuilder.
RelinkInterpartExpression
¶ Relinks the inter part expression using the specific expression from the specific part in case of multiple expression sources.
Signature
RelinkInterpartExpression(partID, expID, sourceID)
Parameters: - partID (
NXOpen.Part
) – - expID (
NXOpen.Expression
) – - sourceID (
NXOpen.Expression
) –
New in version NX7.5.5.
License requirements: wave (“WAVE FUNCTIONALITY”)
- partID (
RelinkWaveFeature¶
-
RelinkerBuilder.
RelinkWaveFeature
¶ Relinks the wave feature using the specific geometry source from the specific part in case of multiple geometry sources.
Signature
RelinkWaveFeature(partID, featID, sourceID)
Parameters: - partID (
NXOpen.Part
) – - featID (
NXOpen.Features.Feature
) – - sourceID (
NXOpen.NXObject
) –
New in version NX7.5.5.
License requirements: wave (“WAVE FUNCTIONALITY”)
- partID (
UpdateSession¶
-
RelinkerBuilder.
UpdateSession
¶ Updates the session.
Signature
UpdateSession()
New in version NX5.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
UpdateSessionWithBreakDelayed¶
-
RelinkerBuilder.
UpdateSessionWithBreakDelayed
¶ Updates the session without immediately breaking wave links or inter part expressions.
Signature
UpdateSessionWithBreakDelayed()
New in version NX8.5.1.
License requirements: wave (“WAVE FUNCTIONALITY”)
Validate¶
-
RelinkerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.