PositioningGroupBuilder Class¶
-
class
NXOpen.Assemblies.
PositioningGroupBuilder
¶ Bases:
NXOpen.Builder
Represents builder class for positioning group which is used to store constraints for design element.
To create a new instance of this class, use
NXOpen.CollaborativeContentManager.CreatePositioningGroupBuilder
Default values.
Property Value MakeActive 1 New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
MakeActive | Returns or sets the option to specify whether a newly created positioning group should be made active after creation or not. |
OwningPositioningTask | Returns or sets the owning positioning task. |
PositioningGroupDataMembers | Returns the members for positioning group |
PositioningGroupName | Returns or sets the name of positioning group. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
MakeActive¶
-
PositioningGroupBuilder.
MakeActive
¶ Returns or sets the option to specify whether a newly created positioning group should be made active after creation or not.
-------------------------------------
Getter Method
Signature
MakeActive()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MakeActive(makeActive)
Parameters: makeActive (bool) – New in version NX10.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
OwningPositioningTask¶
-
PositioningGroupBuilder.
OwningPositioningTask
¶ Returns or sets the owning positioning task.
During creation set method should be called with the positioning task in which new
NXOpen.Assemblies.PositioningGroup
has to be created. During edit operation set method should not be called. An error would be raised if during edit operation set method is called with a positioning task which is different from the owning positioning task ofNXOpen.Assemblies.PositioningGroup
.-------------------------------------
Getter Method
Signature
OwningPositioningTask()
Returns: Return type: NXOpen.Assemblies.PositioningTask
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OwningPositioningTask(positioningTask)
Parameters: positioningTask ( NXOpen.Assemblies.PositioningTask
) – This parameter may not be None.New in version NX10.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
PositioningGroupDataMembers¶
-
PositioningGroupBuilder.
PositioningGroupDataMembers
¶ Returns the members for positioning group
-------------------------------------
Getter Method
Signature
PositioningGroupDataMembers()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX10.0.0.
License requirements: None.
PositioningGroupName¶
-
PositioningGroupBuilder.
PositioningGroupName
¶ Returns or sets the name of positioning group.
The user of this API is responcible to free the text pointer
-------------------------------------
Getter Method
Signature
PositioningGroupName()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PositioningGroupName(nameOfPositioningGroup)
Parameters: nameOfPositioningGroup (str) – New in version NX10.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
Method Detail¶
Validate¶
-
PositioningGroupBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.