ExplodedComponent Class¶
-
class
NXOpen.Assemblies.
ExplodedComponent
¶ Bases:
NXOpen.Assemblies.Component
Represents a
NXOpen.Assemblies.Component
within an explosion.Use the
NXOpen.Assemblies.Explosion
andNXOpen.Assemblies.Component
to create an exploded component.New in version NX9.0.1.
Properties¶
Property | Description |
---|---|
CollaborativeContentType | Returns the collaborative content type of this component. |
Color | Returns or sets the color of the object. |
DesignElementRevision | Returns the NXOpen.PDM.DesignElementRevision that corresponds to this component. |
DesignSubordinateRevision | Returns the NXOpen.PDM.DesignSubordinateRevision that corresponds to this component. |
DirectOwner | Returns the NXOpen.Assemblies.ComponentAssembly which owns this component as a Top Level component. |
DisplayName | Returns the displayable name of the prototype part. |
EmptyPartRefsetName | Returns the name of the reference set which represents the empty set. |
EntirePartRefsetName | Returns the name of the reference set which represents the entire part. |
FixConstraint | Returns a fix NXOpen.Positioning.ComponentConstraint of this component. |
IsBlanked | Returns the blank status of this object. |
IsFixed | Returns the fixed state of this component. |
IsOccurrence | Returns whether this object is an occurrence or not. |
IsSuppressed | Returns the suppressed state of the component in its controlling arrangement. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Parent | Returns the parent of the component. |
Prototype | Returns the prototype of this object if it is an occurrence. |
ReferenceSet | Returns the name of the reference set used for this component |
Subset | Returns the NXOpen.Assemblies.Subset that corresponds to this component. |
SuppressingArrangement | Returns the NXOpen.Assemblies.Arrangement that controls this component’s suppression state. |
Tag | Returns the Tag for this object. |
UsedArrangement | Returns the Arrangement used for this component. |
Methods¶
Method | Description |
---|---|
Blank | Blanks the object. |
CreateEmptyPartFamilyInstanceSelectionCriteria | Creates an empty NXOpen.PartFamily.InstanceSelectionCriteria @return |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteCharacterstics | Removes the input list of characteristics from this object. |
DeleteInstanceUserAttribute | Deletes the first attribute encountered with the given Type, Title and Index. |
DeleteInstanceUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
DeletePartFamilyInstanceSelectionCriteria | Deletes NXOpen.PartFamily.InstanceSelectionCriteria associated with this component |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
DisplayComponentsExact | Sets an array of components to display using the exact representation. |
DisplayComponentsLightweight | Sets an array of components to display using the lightweight representation. |
EstablishIsolatedPositionOverride | Ensures there is an isolated positioning override for the NXOpen.Assemblies.Component in the given part of the given parent. |
EstablishPositionOverride | Ensures there is a positioning override on component in the given part of the given parent. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
FindOccurrence | Given a prototype object, returns the corresponding occurrence in this component @return the occurrence of the prototype in this component |
GetAsRequiredQuantity | Gets the as-required quantity on this component. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetCharacteristics | Get all of the characteristics values on the this object. |
GetChildren | Returns the child components of this component However, it does not return non-geometric components (NGCs) To enable this method to also return NGCs, set the following environment variable: UGII_ALLOW_NGC_IN_UGOPEN=YES @return |
GetComponent | Gets the NXOpen.Assemblies.Component associated with the exploded component. |
GetComponentQuantityType | Gets the quantity type of the components. |
GetComponentRepresentationMode | Returns the representation mode for the component’s bodies. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetConstraints | Returns the :py:class:`NXOpen.Positioning.ComponentConstraint`s directly connected to this component. |
GetDegreesOfFreedom | Returns the NXOpen.Assemblies.DegreesOfFreedom for this component. |
GetDestinationCharacteristics | Returns the destination characteristics from the input object. |
GetExplosion | Gets the NXOpen.Assemblies.Explosion associated with the exploded component. |
GetInstanceBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetInstanceIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetInstanceRealUserAttribute | Gets a real attribute by Title and array Index. |
GetInstanceStringUserAttribute | Gets a string attribute by Title and array Index. |
GetInstanceTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetInstanceUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetInstanceUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetInstanceUserAttributeLock | Determine the lock of the given attribute. |
GetInstanceUserAttributes | Gets all the attributes that have been set on the given object. |
GetInstanceUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerCharacteristic | Get the value of an integer characteristic associated with the input name. |
GetIntegerQuantity | Gets the value of the integer quantity of component. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetLayerOption | Gets the layer option. |
GetNonGeometricState | Gets the component state as Geometric or Non-Geometric. |
GetPartFamilyInstanceSelectionCriteria | Obtains the:py:class:NXOpen.PartFamily.InstanceSelectionCriteria, if it exists. |
GetPosition | Gets the position of a component |
GetPositionOverrideParent | Find the highest level parent in which the position of component is overridden. |
GetPositionOverrideType | Gets the type of the highest level positioning override on the component. |
GetRealAttribute | Gets a real attribute by title. |
GetRealCharacteristic | Get the value of a real characteristic associated with the input name. |
GetRealQuantity | Gets the value of real quantity and corresponding units on this component. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringCharacteristic | Get the value of a string characteristic associated with the input name. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasInstanceUserAttribute | Determines if and attribute with the given Title, Type and array Index is present on the object If the attribute is not an array, the Index is ignored (if this is known beforehand, we recommend setting the Index to -1 to save time). |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
Highlight | Highlights the object. |
IsPositioningIsolated | Get whether positioning for the selected NXOpen.Assemblies.Component is isolated in the specified NXOpen.Assemblies.Arrangement . |
Prints a representation of this object to the system log file. | |
RecallAndListConstraints | Recalls the :py:class:`NXOpen.Positioning.ComponentConstraint`s previously remembered on the part of this component, creating new constraints from them. |
RecallConstraints | Recalls the :py:class:`NXOpen.Positioning.ComponentConstraint`s previously remembered on the part of this component, creating new constraints from them. |
RedisplayObject | Redisplays the object in all views. |
RemovePositionOverride | Removes the highest level positioning override on component in or below the given parent. |
RemoveRememberedConstraints | Remove all the remembered constraints stored on the part of this component. |
RemoveViewDependency | Remove dependency on all views from an object. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetCharacteristic | Set the value of an integer characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. |
SetCharacteristics | Set all of the characteristics values on this object. |
SetInstanceBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetInstanceTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetInstanceUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetInstanceUserAttributeLock | Lock or unlock the given attribute. |
SetLayerOption | Sets the layer option. |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetPartFamilyInstanceSelectionCriteria | Hooks NXOpen.PartFamily.InstanceSelectionCriteria to this component |
SetPositioningIsolated | Set positioning for the selected NXOpen.Assemblies.Component as isolated in the specified NXOpen.Assemblies.Arrangement . |
SetPositioningVaried | Set positioning for the selected :py:class:`NXOpen.Assemblies.Component`s across all possible :py:class:`NXOpen.Assemblies.Arrangement`s. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUsedArrangement | Changes the Arrangement used for this component. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Suppress | Suppresses the component in the ComponentAssembly that contains its controlling Arrangement. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
Unsuppress | Unsuppresses the component in the ComponentAssembly that contains its controlling Arrangement. |
UpdateStructure | Update the assembly structure for this assembly in the context of the displayed part to the specified number of levels, ignoring components already processed by previous calls. |
Property Detail¶
IsOccurrence¶
-
ExplodedComponent.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
ExplodedComponent.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
ExplodedComponent.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
ExplodedComponent.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
ExplodedComponent.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
ExplodedComponent.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
DeleteCharacterstics¶
-
ExplodedComponent.
DeleteCharacterstics
¶ Removes the input list of characteristics from this object.
Signature
DeleteCharacterstics(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
FindObject¶
-
ExplodedComponent.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetCharacteristics¶
-
ExplodedComponent.
GetCharacteristics
¶ Get all of the characteristics values on the this object.
Signature
GetCharacteristics()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetComponent¶
-
ExplodedComponent.
GetComponent
¶ Gets the
NXOpen.Assemblies.Component
associated with the exploded component.Signature
GetComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX9.0.1.
License requirements: assemblies (“ASSEMBLIES MODULE”)
GetDestinationCharacteristics¶
-
ExplodedComponent.
GetDestinationCharacteristics
¶ Returns the destination characteristics from the input object.
Retrieves the description of which destination characteristics to read from the application view and then reads those destination characteristics from the object
- Ports: Reads characteristics from the port.
- RCPs: Attempts to find a port at the RCP, reads characteristics from
the port if it exists, otherwise reads from the stock associated with the rcp.
- Segments: Reads characteristics from the stock associated with the segment.
- Components: Reads characteristics directly from the component.
- Stock: Reads characteristics from the stock or from the stock’s data.
Signature
GetDestinationCharacteristics()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetExplosion¶
-
ExplodedComponent.
GetExplosion
¶ Gets the
NXOpen.Assemblies.Explosion
associated with the exploded component.Signature
GetExplosion()
Returns: Return type: NXOpen.Assemblies.Explosion
New in version NX9.0.1.
License requirements: assemblies (“ASSEMBLIES MODULE”)
GetIntegerCharacteristic¶
-
ExplodedComponent.
GetIntegerCharacteristic
¶ Get the value of an integer characteristic associated with the input name.
Signature
GetIntegerCharacteristic(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: int New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetRealCharacteristic¶
-
ExplodedComponent.
GetRealCharacteristic
¶ Get the value of a real characteristic associated with the input name.
Signature
GetRealCharacteristic(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: float New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetStringCharacteristic¶
-
ExplodedComponent.
GetStringCharacteristic
¶ Get the value of a string characteristic associated with the input name.
Signature
GetStringCharacteristic(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: str New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
Print¶
-
ExplodedComponent.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetCharacteristic¶
-
ExplodedComponent.
SetCharacteristic
¶ Overloaded method SetCharacteristic
SetCharacteristic(name, value)
SetCharacteristic(name, value)
SetCharacteristic(name, value)
-------------------------------------
Set the value of an integer characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to integer if it’s type is not integer.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- value (int) –
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Set the value of an real characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to real if it’s type is not real.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- value (float) –
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Set the value of an string characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to string if it’s type is not string.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- value (str) – NOTE: The full Unicode character set is not supported for this parameter.
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
SetCharacteristics¶
-
ExplodedComponent.
SetCharacteristics
¶ Set all of the characteristics values on this object.
Signature
SetCharacteristics(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
SetName¶
-
ExplodedComponent.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.