TitleBlockCollection Class¶
-
class
NXOpen.Annotations.
TitleBlockCollection
¶ Bases:
object
Represents a collection of
NXOpen.Annotations.TitleBlock
.To obtain an instance of this class, refer to
NXOpen.Drafting.DraftingApplicationManager
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
CreateCellBuilder | Creates a cell builder @return |
CreateDefineTitleBlockBuilder | Creates a NXOpen.Annotations.DefineTitleBlockBuilder . |
CreateEditTitleBlockBuilder | Creates a NXOpen.Annotations.EditTitleBlockBuilder . |
Method Detail¶
CreateCellBuilder¶
-
TitleBlockCollection.
CreateCellBuilder
¶ Creates a cell builder
Signature
CreateCellBuilder(object, isLocked, contentType, value, label, canLockStatusChange)
Parameters: - object (
NXOpen.DisplayableObject
) – - isLocked (bool) –
- contentType (int) –
- value (str) –
- label (str) –
- canLockStatusChange (bool) –
Returns: Return type: New in version NX8.0.0.
License requirements: None.
- object (
CreateDefineTitleBlockBuilder¶
-
TitleBlockCollection.
CreateDefineTitleBlockBuilder
¶ Creates a
NXOpen.Annotations.DefineTitleBlockBuilder
.This builder provides functions to create a new title block from tabular notes or add/remove tabular notes from existing title block. It also permits user to edit label and lock status of cells. If you want to edit values of cells in existing title block, please use
NXOpen.Annotations.EditTitleBlockBuilder
.Signature
CreateDefineTitleBlockBuilder(titleblock)
Parameters: titleblock ( NXOpen.Annotations.TitleBlock
) –Returns: Return type: NXOpen.Annotations.DefineTitleBlockBuilder
New in version NX8.0.0.
License requirements: None.
CreateEditTitleBlockBuilder¶
-
TitleBlockCollection.
CreateEditTitleBlockBuilder
¶ Creates a
NXOpen.Annotations.EditTitleBlockBuilder
.This builder provides functions for editing values of unlocked cells in one or more title blocks. If you want to create a new title block from tabular notes or add/remove tabular notes from existing title block, please use
NXOpen.Annotations.DefineTitleBlockBuilder
.Signature
CreateEditTitleBlockBuilder(titleBlocks)
Parameters: titleBlocks (list of NXOpen.Annotations.TitleBlock
) –Returns: Return type: NXOpen.Annotations.EditTitleBlockBuilder
New in version NX8.0.0.
License requirements: None.