TableCellStyleBuilderFormatType Enumeration¶
NXOpen.Annotations.TableCellStyleBuilder.FormatType is an alias for NXOpen.Annotations.TableCellStyleBuilderFormatType
-
class
NXOpen.Annotations.
TableCellStyleBuilderFormatType
¶ Bases:
object
the valid cell format types
Deprecated since version NX10.0.0: Use
NXOpen.Annotations.TableCellStyleBuilderCellFormatTypes
instead.Enum Members
Enum Member Enum Member Description Text Float Fixed General Monetary Comma FractionHalfSize FractionThreeQuarterSize FractionFullSize DegreesDegreeUnits DegreesDegreesRadianUnits RadiansPercent Degrees RadiansHex Logic DateDmy DateDm DateMy DateMdy DateYmd DateY4md DateDmyDot TimeHm TimeHms Hidden Custom -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-