TableCellStyleBuilderCellFormatTypes Enumeration¶
NXOpen.Annotations.TableCellStyleBuilder.CellFormatTypes is an alias for NXOpen.Annotations.TableCellStyleBuilderCellFormatTypes
-
class
NXOpen.Annotations.
TableCellStyleBuilderCellFormatTypes
¶ Bases:
object
the cell format types
Enum Members
Enum Member Enum Member Description Text TextFloat FloatFixed FixedGeneral GeneralMonetary MonetaryComma CommaFractionHalfSize Fraction half sizeFractionThreeQuarterSize Fraction three quarter sizeFractionFullSize Fraction full sizeDegreesDegreeUnits DegreesDegreesRadianUnits RadiansPercent PercentDegrees RadiansHex HexLogic LogicHidden HiddenCustom CustomDate DateTime TimeDateTime Date-Time-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-