SearchModelView Class¶
-
class
NXOpen.Annotations.
SearchModelView
¶ Bases:
NXOpen.ModelingView
Represents a search model view
To create or edit an instance of this class, use
NXOpen.Annotations.SearchModelViewBuilder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AbsoluteOrigin | Returns the view origin in absolute space. |
ActiveDynamicSection | Returns or sets the active dynamic section object in the modeling view. |
DisplaySectioningToggle | Returns or sets the toggle between enabling or disabling the Dynamic Sectioning viewing |
IsMirrored | Returns a flag indicating whether the model view is mirrored |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
LockRotations | Returns or sets the Lock Rotations toggle state of a view. |
Matrix | Returns the view matrix. |
Name | Returns the custom name of the object. |
Origin | Returns the view origin. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
RenderingStyle | Returns or sets the rendering style of the view. |
Scale | Returns the view scale |
SyncViews | Returns or sets the Synchronized Views toggle state of a view. |
Tag | Returns the Tag for this object. |
TriadVisibility | Returns or sets the visibility of the view triad in the view. |
WcsVisibility | Returns or sets the visibility of the WCS in the view. |
Methods¶
Method | Description |
---|---|
AskVisibleObjects | Returns an array of objects visible in a view @return The array of visible objects |
Concatenate | Concatenates the given translation with the previous viewing transformation of the specified view. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
Expand | Expands the specified view to fill as much of the layout which contains the view as possible, without changing the aspect ratio of the view. |
ExpandCollapseNode | Expand or collapse the node for the specified Model View in the Part Navigator. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
Fit | Adjusts the bounds of a given view so that it fully encompasses the extents of the model geometry. |
FitAfterShowOrHide | Adjusts the bounds of a given view conditionally so that it fully encompasses the extents of the model geometry. |
FitToObjects | Adjusts the bounds of a given view so that it fully encompasses the extents of the given objects. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetAxis | Returns one of the view axes. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetDisplaySectioning | To adjust and orient the Sectioning planes as a quick display trick. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
IsDynamicSectionVisible | Returns if the specified dynamic section object is visible in this view. |
MakeWork | Makes the given view the work view. |
Orient | Changes the view orientation relative to the specified absolute coordinate system. |
Prints a representation of this object to the system log file. | |
Regenerate | Regenerates the display of given view. |
Restore | Restores a view to its last remembered rotation, scale and translation. |
Rotate | Rotates the view by concatenating the given matrix to the existing rotation matrix of the view. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetDisplaySectioning | To adjust and orient the Sectioning planes as a quick display trick. |
SetDynamicSectionVisible | Sets the specified dynamic section object is visible/invisible in this view. |
SetName | Sets the custom name of the object. |
SetOrigin | Moves the given position to the center of the view. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetRotationTranslationScale | Sets the rotation, translation and scale of the specified view. |
SetScale | Sets the scale of the specified view to the desired scale factor. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
SnapToClosestCannedOrientation | Changes the orientation of the given view to the orientation of the canned view whose orientation is the closest to that of the given view. |
SnapToVariantCannedOrientation | Similar to NXOpen.View.SnapToClosestCannedOrientation except it changes the orientation of the given view to the orientation of some canned view variant based on I-deas’s ‘snapview’ logic whose orientation is the closest to one of the six orthographic and eight flavors of trimetric views. |
UpdateCustomSymbols | Updates custom symbol in a drawing member view or drawing sheet |
UpdateDisplay | Updates the display of given view, as needed. |
UseDefaultLights | Changes the set of lights used in the given view to the Default set, which for now is the Scene Ambient, Scene Left Top and Scene Right Top lights. |
UseSceneLights | Changes the set of lights used in the given view to the Scene set, which for now includes the eight predefined scene lights (including the Scene Ambient light). |
Zoom | Scales the specified view to a desired relative scale. |
ZoomAboutPoint | Scales the specified view such that the given scale_about_point does not move. |
ZoomByRectangle | Scales the specified view such that the specified rectangle is as large as possible while being fully contained within the viewport. |
Property Detail¶
IsOccurrence¶
-
SearchModelView.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
SearchModelView.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
SearchModelView.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
SearchModelView.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
SearchModelView.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
SearchModelView.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
FindObject¶
-
SearchModelView.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Print¶
-
SearchModelView.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
SearchModelView.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.