PmiFilterCollection Class¶
-
class
NXOpen.Annotations.
PmiFilterCollection
¶ Bases:
object
Represents the collection of all PMI filters in the part.
To obtain an instance of this class, refer to
NXOpen.Annotations.AnnotationManager
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateByPartsFilter | Creates a PMI filter defined by a set of components @return |
CreateByTypesFilter | Creates a PMI filter defines by a set of PMI types. |
CreateByViewsFilter | Creates a PMI filter defined by a set of model views. |
Method Detail¶
CreateByPartsFilter¶
-
PmiFilterCollection.
CreateByPartsFilter
¶ Creates a PMI filter defined by a set of components
Signature
CreateByPartsFilter(componentMethod, components)
Parameters: - componentMethod (
NXOpen.Annotations.PmiFilterComponentMethod
) – Specifies the component method applied to the components - components (list of
NXOpen.Assemblies.Component
) – Specifies the components in which the filter applies
Returns: Return type: New in version NX4.0.0.
License requirements: geometric_tol (“GDT”)
- componentMethod (
CreateByTypesFilter¶
-
PmiFilterCollection.
CreateByTypesFilter
¶ Creates a PMI filter defines by a set of PMI types.
Signature
CreateByTypesFilter(componentMethod, components, types)
Parameters: - componentMethod (
NXOpen.Annotations.PmiFilterComponentMethod
) – Specifies the component method applied to the components - components (list of
NXOpen.Assemblies.Component
) – Specifies the components in which the filter applies - types (list of
NXOpen.Annotations.PmiFilterByTypeType
) – Specifies the types in which the filter applies
Returns: Return type: New in version NX4.0.0.
License requirements: geometric_tol (“GDT”)
- componentMethod (
CreateByViewsFilter¶
-
PmiFilterCollection.
CreateByViewsFilter
¶ Creates a PMI filter defined by a set of model views.
Signature
CreateByViewsFilter(componentMethod, components, views)
Parameters: - componentMethod (
NXOpen.Annotations.PmiFilterComponentMethod
) – Specifies the component method applied to the components - components (list of
NXOpen.Assemblies.Component
) – Specifies the components in which the filter applies - views (list of str) – Specified the views in which the filter applies NOTE: The full Unicode character set is not supported for this parameter.
Returns: Return type: New in version NX4.0.0.
License requirements: geometric_tol (“GDT”)
- componentMethod (