LeaderData Class¶
-
class
NXOpen.Annotations.
LeaderData
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.LeaderData
.This class is used to construct the definition for a single leader object.
To create a new instance of this class, use
NXOpen.Annotations.AnnotationManager.CreateLeaderData
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Arrowhead | Returns or sets the arrowhead |
DatumOnDotTerminatedArrowhead | Returns or sets the datum arrowhead type for the datum portion of a datum on dot terminated leader |
DatumOnDotTerminatedEndPoint | Returns or sets the datum end point for the leader segment of the datum portion of a datum on dot terminated leadet |
DatumOnDotTerminatedStartPoint | Returns or sets the datum start point for the leader segment of the datum portion of a datum on dot terminated leader |
Jogs | Returns the jogs |
Leader | Returns the leader |
LeaderPerpendicular | Returns or sets the perpendicular relationship between the first segment and attachement object |
Perpendicular | Returns or sets the perpendicular relationship between the first segment and stub |
StubSide | Returns or sets the stub side |
StubSize | Returns or sets the stub size |
Tag | Returns the Tag for this object. |
TerminatorType | Returns or sets the terminator type |
VerticalAttachment | Returns or sets the vertical attachment |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LeaderDataArrowheadType Enumeration | the set of arrowhead types used to define a leader arrowhead |
LeaderDataLeaderType Enumeration | the set of datatypes used to define the types of leaders that can be applied to an annotation |
Property Detail¶
Arrowhead¶
-
LeaderData.
Arrowhead
¶ Returns or sets the arrowhead
-------------------------------------
Getter Method
Signature
Arrowhead()
Returns: Return type: NXOpen.Annotations.LeaderDataArrowheadType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Arrowhead(arrowhead)
Parameters: arrowhead ( NXOpen.Annotations.LeaderDataArrowheadType
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
DatumOnDotTerminatedArrowhead¶
-
LeaderData.
DatumOnDotTerminatedArrowhead
¶ Returns or sets the datum arrowhead type for the datum portion of a datum on dot terminated leader
-------------------------------------
Getter Method
Signature
DatumOnDotTerminatedArrowhead()
Returns: Return type: NXOpen.Annotations.LeaderDataArrowheadType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DatumOnDotTerminatedArrowhead(arrowhead)
Parameters: arrowhead ( NXOpen.Annotations.LeaderDataArrowheadType
) –New in version NX9.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
DatumOnDotTerminatedEndPoint¶
-
LeaderData.
DatumOnDotTerminatedEndPoint
¶ Returns or sets the datum end point for the leader segment of the datum portion of a datum on dot terminated leadet
-------------------------------------
Getter Method
Signature
DatumOnDotTerminatedEndPoint()
Returns: Return type: NXOpen.Point3d
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DatumOnDotTerminatedEndPoint(endpoint)
Parameters: endpoint ( NXOpen.Point3d
) –New in version NX9.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
DatumOnDotTerminatedStartPoint¶
-
LeaderData.
DatumOnDotTerminatedStartPoint
¶ Returns or sets the datum start point for the leader segment of the datum portion of a datum on dot terminated leader
-------------------------------------
Getter Method
Signature
DatumOnDotTerminatedStartPoint()
Returns: Return type: NXOpen.Point3d
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DatumOnDotTerminatedStartPoint(startpoint)
Parameters: startpoint ( NXOpen.Point3d
) –New in version NX9.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
Jogs¶
-
LeaderData.
Jogs
¶ Returns the jogs
-------------------------------------
Getter Method
Signature
Jogs()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX6.0.0.
License requirements: None.
Leader¶
-
LeaderData.
Leader
¶ Returns the leader
-------------------------------------
Getter Method
Signature
Leader()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX6.0.0.
License requirements: None.
LeaderPerpendicular¶
-
LeaderData.
LeaderPerpendicular
¶ Returns or sets the perpendicular relationship between the first segment and attachement object
-------------------------------------
Getter Method
Signature
LeaderPerpendicular()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LeaderPerpendicular(isLeaderPerpendicular)
Parameters: isLeaderPerpendicular (bool) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
Perpendicular¶
-
LeaderData.
Perpendicular
¶ Returns or sets the perpendicular relationship between the first segment and stub
-------------------------------------
Getter Method
Signature
Perpendicular()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Perpendicular(isPerpendicular)
Parameters: isPerpendicular (bool) – New in version NX7.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
StubSide¶
-
LeaderData.
StubSide
¶ Returns or sets the stub side
-------------------------------------
Getter Method
Signature
StubSide()
Returns: Return type: NXOpen.Annotations.LeaderSide
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StubSide(stubSide)
Parameters: stubSide ( NXOpen.Annotations.LeaderSide
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
StubSize¶
-
LeaderData.
StubSize
¶ Returns or sets the stub size
-------------------------------------
Getter Method
Signature
StubSize()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StubSize(stubSize)
Parameters: stubSize (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
TerminatorType¶
-
LeaderData.
TerminatorType
¶ Returns or sets the terminator type
-------------------------------------
Getter Method
Signature
TerminatorType()
Returns: Return type: NXOpen.Annotations.LeaderDataLeaderType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TerminatorType(terminatorType)
Parameters: terminatorType ( NXOpen.Annotations.LeaderDataLeaderType
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
VerticalAttachment¶
-
LeaderData.
VerticalAttachment
¶ Returns or sets the vertical attachment
-------------------------------------
Getter Method
Signature
VerticalAttachment()
Returns: Return type: NXOpen.Annotations.LeaderVerticalAttachment
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VerticalAttachment(verticalAttachment)
Parameters: verticalAttachment ( NXOpen.Annotations.LeaderVerticalAttachment
) –New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
LeaderData.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.