LeaderDataArrowheadType Enumeration¶
NXOpen.Annotations.LeaderData.ArrowheadType is an alias for NXOpen.Annotations.LeaderDataArrowheadType
-
class
NXOpen.Annotations.
LeaderDataArrowheadType
¶ Bases:
object
the set of arrowhead types used to define a leader arrowhead
Enum Members
Enum Member Enum Member Description ClosedArrow Closed arrowhead typeClosedSolidArrow Closed solid arrowhead typeOpenArrow Open arrowhead typeFilledArrow Filled arrowhead typeClosedDoubleArrow Closed double arrowhead typeClosedDoubleSolidArrow Closed double solid arrowhead typeOpenDoubleArrow Open double arrowhead typeFilledDoubleArrow Filled double arrowhead typeNone No terminating symbolOrigin Origin symbolCross Cross symbolIntegral Integral symbolDot Dot symbolFilledDot Filled dot symbolSquare Square symbolFilledSquare Filled square symbolDatum Datum symbolFilledDatum Filled datum symbolTopOpenArrow Top open arrowheadBottomOpenArrow bottom open arrowheadTopFilledArrow top filled arrowheadBottomFilledArrow bottom filled arrowhead-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-