HoleTableSettingsWorkflowBuilder Class¶
-
class
NXOpen.Annotations.
HoleTableSettingsWorkflowBuilder
¶ Bases:
NXOpen.Annotations.TabularNoteStyleBuilder
Represents a
NXOpen.Annotations.HoleTableSettingsWorkflowBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AutomaticUpdate | Returns or sets the automatic update |
LockTableContents | Returns or sets the lock table contents |
LockTableFormat | Returns or sets the lock table format |
ShowLockedDeletedContent | Returns or sets the locked deleted row method |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
Validate¶
-
HoleTableSettingsWorkflowBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.