TabularNoteStyleBuilder Class¶
-
class
NXOpen.Annotations.
TabularNoteStyleBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.TabularNoteStyleBuilder
.New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AutomaticUpdate | Returns or sets the automatic update |
LockTableContents | Returns or sets the lock table contents |
LockTableFormat | Returns or sets the lock table format |
ShowLockedDeletedContent | Returns or sets the locked deleted row method |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TabularNoteStyleBuilderShowLockedDeletedRowMethod Enumeration | the valid locked deleted row methods |
Property Detail¶
AutomaticUpdate¶
-
TabularNoteStyleBuilder.
AutomaticUpdate
¶ Returns or sets the automatic update
-------------------------------------
Getter Method
Signature
AutomaticUpdate()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AutomaticUpdate(automaticUpdate)
Parameters: automaticUpdate (bool) – New in version NX8.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
LockTableContents¶
-
TabularNoteStyleBuilder.
LockTableContents
¶ Returns or sets the lock table contents
-------------------------------------
Getter Method
Signature
LockTableContents()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LockTableContents(lockedTableContents)
Parameters: lockedTableContents (bool) – New in version NX8.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
LockTableFormat¶
-
TabularNoteStyleBuilder.
LockTableFormat
¶ Returns or sets the lock table format
-------------------------------------
Getter Method
Signature
LockTableFormat()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LockTableFormat(lockedTableFormat)
Parameters: lockedTableFormat (bool) – New in version NX8.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
ShowLockedDeletedContent¶
-
TabularNoteStyleBuilder.
ShowLockedDeletedContent
¶ Returns or sets the locked deleted row method
-------------------------------------
Getter Method
Signature
ShowLockedDeletedContent()
Returns: Return type: NXOpen.Annotations.TabularNoteStyleBuilderShowLockedDeletedRowMethod
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowLockedDeletedContent(showLockedDeletedContent)
Parameters: showLockedDeletedContent ( NXOpen.Annotations.TabularNoteStyleBuilderShowLockedDeletedRowMethod
) –New in version NX8.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
TabularNoteStyleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.