EditLeaderBuilder Class¶
-
class
NXOpen.Annotations.
EditLeaderBuilder
¶ Bases:
NXOpen.Builder
Represents a builder that provides an interface to adding and editing leaders to table entities
To create a new instance of this class, use
NXOpen.Annotations.AnnotationManager.CreateEditLeaderBuilder
New in version NX6.0.1.
Properties¶
Property | Description |
---|---|
Leader | Returns the Annotations.LeaderBuilder for the annotation |
Origin | Returns the Annotations.OriginBuilder for the annotation |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Leader¶
-
EditLeaderBuilder.
Leader
¶ Returns the
Annotations.LeaderBuilder
for the annotation-------------------------------------
Getter Method
Signature
Leader()
Returns: Return type: NXOpen.Annotations.LeaderBuilder
New in version NX6.0.1.
License requirements: None.
Origin¶
-
EditLeaderBuilder.
Origin
¶ Returns the
Annotations.OriginBuilder
for the annotation-------------------------------------
Getter Method
Signature
Origin()
Returns: Return type: NXOpen.Annotations.OriginBuilder
New in version NX6.0.1.
License requirements: None.
Method Detail¶
Validate¶
-
EditLeaderBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.