DiameterRadiusPreferences Class¶
-
class
NXOpen.Annotations.
DiameterRadiusPreferences
¶ Bases:
NXOpen.TransientObject
Represents diameter and radius preferences
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
DiameterSymbol | Returns or sets the diameter symbol |
DiameterSymbolText | Returns or sets the symbol text for user defined diameter symbol |
DistanceBetweenSymbolAndDimensionText | Returns or sets the distance between diameter/radius symbol and dimension text |
FoldedRadiusAngle | Returns or sets the interior angle for folded radius type dimension |
LeaderStub | Returns or sets the leader stub relative to diameter/radius dimension text |
RadiusSymbol | Returns or sets the radius symbol |
RadiusSymbolText | Returns or sets the symbol text for user defined radius symbol |
SymbolPlacement | Returns or sets the diameter/radius symbol placement relative to the dimension text |
Property Detail¶
DiameterSymbol¶
-
DiameterRadiusPreferences.
DiameterSymbol
¶ Returns or sets the diameter symbol
-------------------------------------
Getter Method
Signature
DiameterSymbol()
Returns: Diameter symbol Return type: NXOpen.Annotations.DiameterSymbol
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DiameterSymbol(symbol)
Parameters: symbol ( NXOpen.Annotations.DiameterSymbol
) – New diameter symbolNew in version NX4.0.0.
License requirements: None.
DiameterSymbolText¶
-
DiameterRadiusPreferences.
DiameterSymbolText
¶ Returns or sets the symbol text for user defined diameter symbol
-------------------------------------
Getter Method
Signature
DiameterSymbolText()
Returns: Symbol text Return type: str New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DiameterSymbolText(symbolText)
Parameters: symbolText (str) – New symbol text New in version NX4.0.0.
License requirements: None.
DistanceBetweenSymbolAndDimensionText¶
-
DiameterRadiusPreferences.
DistanceBetweenSymbolAndDimensionText
¶ Returns or sets the distance between diameter/radius symbol and dimension text
-------------------------------------
Getter Method
Signature
DistanceBetweenSymbolAndDimensionText()
Returns: Distance between symbol and dimension text Return type: float New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceBetweenSymbolAndDimensionText(symbolToDimensionTextDistance)
Parameters: symbolToDimensionTextDistance (float) – New distance between symbol and dimension text New in version NX4.0.0.
License requirements: None.
FoldedRadiusAngle¶
-
DiameterRadiusPreferences.
FoldedRadiusAngle
¶ Returns or sets the interior angle for folded radius type dimension
-------------------------------------
Getter Method
Signature
FoldedRadiusAngle()
Returns: Folded radius angle Return type: float New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FoldedRadiusAngle(foldedRadiusAngle)
Parameters: foldedRadiusAngle (float) – New folded radius angle New in version NX4.0.0.
License requirements: None.
LeaderStub¶
-
DiameterRadiusPreferences.
LeaderStub
¶ Returns or sets the leader stub relative to diameter/radius dimension text
-------------------------------------
Getter Method
Signature
LeaderStub()
Returns: Leader stub relative to dimension text Return type: NXOpen.Annotations.DiameterRadiusLeaderStub
New in version NX4.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Annotations.DimensionPreferences.TextPosition
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
LeaderStub(leaderStub)
Parameters: leaderStub ( NXOpen.Annotations.DiameterRadiusLeaderStub
) – New leader stub relative to dimension textNew in version NX4.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Annotations.DimensionPreferences.TextPosition
instead.License requirements: None.
RadiusSymbol¶
-
DiameterRadiusPreferences.
RadiusSymbol
¶ Returns or sets the radius symbol
-------------------------------------
Getter Method
Signature
RadiusSymbol()
Returns: Radius symbol Return type: NXOpen.Annotations.RadiusSymbol
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadiusSymbol(symbol)
Parameters: symbol ( NXOpen.Annotations.RadiusSymbol
) – New radius symbolNew in version NX4.0.0.
License requirements: None.
RadiusSymbolText¶
-
DiameterRadiusPreferences.
RadiusSymbolText
¶ Returns or sets the symbol text for user defined radius symbol
-------------------------------------
Getter Method
Signature
RadiusSymbolText()
Returns: Symbol text Return type: str New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadiusSymbolText(symbolText)
Parameters: symbolText (str) – New symbol text New in version NX4.0.0.
License requirements: None.
SymbolPlacement¶
-
DiameterRadiusPreferences.
SymbolPlacement
¶ Returns or sets the diameter/radius symbol placement relative to the dimension text
-------------------------------------
Getter Method
Signature
SymbolPlacement()
Returns: Symbol placement relative to dimension text Return type: NXOpen.Annotations.DiameterRadiusSymbolPlacement
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SymbolPlacement(symbolPlacement)
Parameters: symbolPlacement ( NXOpen.Annotations.DiameterRadiusSymbolPlacement
) – New symbol placement relative to dimension textNew in version NX4.0.0.
License requirements: None.
Method Detail¶
Dispose¶
-
DiameterRadiusPreferences.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX4.0.0.
License requirements: None.