BoundaryBuilder Class¶
-
class
NXOpen.Annotations.
BoundaryBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
This builder contains the boundaries that define a crosshatch pattern
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
CurveBoundaries | Returns the curve boundaries |
DistanceTolerance | Returns or sets the distance tolerance |
SelectionType | Returns or sets the selection type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetView | The boundary view @return Drafting view |
SetView | The boundary view |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BoundaryBuilderSelectionMethod Enumeration | This enum represents the methods for selecting boundaries |
Property Detail¶
CurveBoundaries¶
-
BoundaryBuilder.
CurveBoundaries
¶ Returns the curve boundaries
-------------------------------------
Getter Method
Signature
CurveBoundaries()
Returns: Return type: NXOpen.SectionList
New in version NX6.0.0.
License requirements: None.
DistanceTolerance¶
-
BoundaryBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
SelectionType¶
-
BoundaryBuilder.
SelectionType
¶ Returns or sets the selection type
-------------------------------------
Getter Method
Signature
SelectionType()
Returns: Return type: NXOpen.Annotations.BoundaryBuilderSelectionMethod
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectionType(type)
Parameters: type ( NXOpen.Annotations.BoundaryBuilderSelectionMethod
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
GetView¶
-
BoundaryBuilder.
GetView
¶ The boundary view
Signature
GetView()
Returns: Drafting view Return type: NXOpen.View
New in version NX6.0.0.
License requirements: None.
SetView¶
-
BoundaryBuilder.
SetView
¶ The boundary view
Signature
SetView(view)
Parameters: view ( NXOpen.View
) – Drafting viewNew in version NX6.0.0.
License requirements: None.
Validate¶
-
BoundaryBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.