BaseChamferDimensionBuilder Class¶
-
class
NXOpen.Annotations.
BaseChamferDimensionBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Annotations.BaseChamferDimension
builderThis is an abstract class and cannot be instantiated.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AppendedText | Returns the appended text |
FirstAssociativity | Returns the first associativity |
Inherit | Returns the inherit |
Orientation | Returns or sets the orientation of linear chamfer dimension |
Origin | Returns the origin |
SecondAssociativity | Returns the second associativity |
Style | Returns the style |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AppendedText¶
-
BaseChamferDimensionBuilder.
AppendedText
¶ Returns the appended text
-------------------------------------
Getter Method
Signature
AppendedText()
Returns: Return type: NXOpen.Annotations.AppendedTextBuilder
New in version NX9.0.0.
License requirements: None.
FirstAssociativity¶
-
BaseChamferDimensionBuilder.
FirstAssociativity
¶ Returns the first associativity
-------------------------------------
Getter Method
Signature
FirstAssociativity()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX9.0.0.
License requirements: None.
Inherit¶
-
BaseChamferDimensionBuilder.
Inherit
¶ Returns the inherit
-------------------------------------
Getter Method
Signature
Inherit()
Returns: Return type: NXOpen.Annotations.SelectDimension
New in version NX9.0.0.
License requirements: None.
Orientation¶
-
BaseChamferDimensionBuilder.
Orientation
¶ Returns or sets the orientation of linear chamfer dimension
-------------------------------------
Getter Method
Signature
Orientation()
Returns: Return type: NXOpen.Annotations.ChamferOrientationType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Orientation(orientation)
Parameters: orientation ( NXOpen.Annotations.ChamferOrientationType
) –New in version NX9.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
Origin¶
-
BaseChamferDimensionBuilder.
Origin
¶ Returns the origin
-------------------------------------
Getter Method
Signature
Origin()
Returns: Return type: NXOpen.Annotations.OriginBuilder
New in version NX9.0.0.
License requirements: None.
SecondAssociativity¶
-
BaseChamferDimensionBuilder.
SecondAssociativity
¶ Returns the second associativity
-------------------------------------
Getter Method
Signature
SecondAssociativity()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX9.0.0.
License requirements: None.
Style¶
-
BaseChamferDimensionBuilder.
Style
¶ Returns the style
-------------------------------------
Getter Method
Signature
Style()
Returns: Return type: NXOpen.Annotations.StyleBuilder
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
BaseChamferDimensionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.