ChamferOrientationType Enumeration¶
-
class
NXOpen.Annotations.
ChamferOrientationType
¶ Bases:
object
Specifies the linear chamfer dimension orientation Enum Members
Enum Member Enum Member Description Horizontal default (same as the adjacent edge)Vertical perpendicular with defaultParallel parallel to the chamfer line itself-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-