Matrix rendering
There are two system properties that define the maximum number of cells in a Traceability matrix or a Variants comparison matrix.
com.siemens.polarion.ui.matrix.hardLimit
This property sets the maximum allowed number of matrix cells.
Example: com.siemens.polarion.ui.matrix.hardLimit=50000 sets a limit of fifty thousand cells.
com.siemens.polarion.ui.matrix.softLimit
This property defines the number of cells which, if exceeded, triggers a warning before displaying the matrix.
Example: com.siemens.polarion.ui.matrix.softLimit=10000 specifies that if matrix queries will result in at least ten thousand cells, which could impact system performance, a warning message will be shown to users, who can then choose to cancel or proceed.