Display a Chart
To display the diagram picture of a Chart on the HTML page, click on the toolbar .
Select the Chart which you would like to show. Click OK.
Enter the caption which the HtmlReport shows below the Chart.
Enter the Image width with which the HtmlReport shows the picture of the object. You can also enter an asterisk (*) for either the width or the height to ensure that the image will not be distorted.
Enter the image height with which the HtmlReport shows the picture of the object. You can also enter an asterisk (*) for either the width or the height to ensure that the image will not be distorted.
Instead, you can also type in the instructions that correspond to the settings you can enter into the dialog.
[StationChart] -- our Chart is called StationChart |
Related Topic
Related Topics
Select an Object or an Object Attribute to be Displayed on the HTML PageDisplay Statistics Values of an Object as a Table in the Report
Display a Drain
Display a Broker
Display a DataTable or a List Object
Display a Table from the SQLite Interface
Display a GanttChart
Display a Frame
Display an AttributeExplorer
Display a FileLink
Display a Variable
Display an Object of Type Display
Display a Check Box
Display a Dropdown List
Display a Method
Display a HtmlReport
Display a Picture of a 3D Scene