Display an AttributeExplorer
To display the attribute table of an AttributeExplorer on the HTML page, click on the toolbar .
You can type in the following instructions to set the columns to be displayed.
[AttributeExplorer] |
Related Topic
Related Topics
Select an Object or an Object Attribute to be Displayed on the HTML PageDisplay Statistics Values of an Object as a Table in the Report
Display a Drain
Display a Broker
Display a DataTable or a List Object
Display a Table from the SQLite Interface
Display a Chart
Display a GanttChart
Display a Frame
Display a FileLink
Display a Variable
Display an Object of Type Display
Display a Check Box
Display a Dropdown List
Display a Method
Display a HtmlReport
Display a Picture of a 3D Scene