Distance
Syntax
<MU-Path>.Distance:length |
The attribute Distance sets the Distance from which on the Transporter calls the Distance to prevent the MUs from getting too close to each other or moving away too far from each other. You can enter a value greater than 0.
Data Type of the Value You Can Assign
You can assign a value of data type length.
Example
.MUs.MyTransporter.Distance :=1 |
Related Topics
Attributes of the TransporterAcceleration (Transporter)
AccelerationEnabled (Transporter)
Accumulating (Transporter)
AutomaticRouting (Transporter)
Backwards (Transporter)
BatBasicCons
BatCapacity
BatCharge
BatCharging
BatChargeCtrl
BatChargeCurrent
BatDriveCons
BatReserve
BatteryUsed
BwEntranceCtrl (Transporter)
BwEntranceCtrlFront (Transporter)
BwEntranceCtrlRear (Transporter)
BwExitCtrl (Transporter)
BwExitCtrlFront (Transporter)
BwExitCtrlRear (Transporter)
Capacity (Transporter)
CollisionCtrl (Transporter)
CurrentSpeed (Transporter)
Deceleration (Transporter)
DefaultCurveRadius
DestCtrl
Destination (Transporter)
DestinationListRow
DistanceCtrl
DriveCtrl
DrivingHome
EntranceCtrl (Transporter)
EntranceCtrlFront (Transporter)
EntranceCtrlRear (Transporter)
ExitCtrl (Transporter)
ExitCtrlFront (Transporter)
ExitCtrlRear (Transporter)
Failed (Transporter)
HasOrder
InitCtrl (Transporter)
IsIdle
IsTractor
LoadBayAcceleration
LoadBayAccelerationEnabled
LoadBayBackwards
LoadBayCurrentSpeed
LoadBayLength (Transporter)
LoadBayDeceleration
LoadBaySpeed (Transporter)
LoadBaySpeedCtrl
LoadBayType
Pause (Transporter)
RotationSpeed
RouteWeightingAttr (Transporter)
RoutingCtrl
ShiftCalendarObject (Transporter)
Speed (Transporter)
SpeedCtrl (Transporter)
StartDelayDuration
TargetDistance
TargetPosition
XDim (Transporter)
YDim (Transporter)
ZDim (Transporter)