CollisionCtrl (Transporter)
Syntax
<MU-Path>.CollisionCtrl:method |
The attribute CollisionCtrl designates a Method object, the Collision control, which Plant Simulation activates, when a faster Transporter collides with a slower one, i.e., the following Transporter drives faster than the one driving ahead of it and the distance between them is 0.
Data Type of the Value You Can Assign
You can assign a value of data type method.
Example
if .MUs.MyTransporter.CollisionCtrl = VOID |
-- myCollisionControl |
Related Topic
Related Topics
Attributes of the TransporterAcceleration (Transporter)
AccelerationEnabled (Transporter)
Accumulating (Transporter)
AutomaticRouting (Transporter)
Backwards (Transporter)
BatBasicCons
BatCapacity
BatCharge
BatCharging
BatChargeCtrl
BatChargeCurrent
BatDriveCons
BatReserve
BatteryUsed
BwEntranceCtrl (Transporter)
BwEntranceCtrlFront (Transporter)
BwEntranceCtrlRear (Transporter)
BwExitCtrl (Transporter)
BwExitCtrlFront (Transporter)
BwExitCtrlRear (Transporter)
Capacity (Transporter)
CurrentSpeed (Transporter)
Deceleration (Transporter)
DefaultCurveRadius
DestCtrl
Destination (Transporter)
DestinationListRow
Distance
DistanceCtrl
DriveCtrl
DrivingHome
EntranceCtrl (Transporter)
EntranceCtrlFront (Transporter)
EntranceCtrlRear (Transporter)
ExitCtrl (Transporter)
ExitCtrlFront (Transporter)
ExitCtrlRear (Transporter)
Failed (Transporter)
HasOrder
InitCtrl (Transporter)
IsIdle
IsTractor
LoadBayAcceleration
LoadBayAccelerationEnabled
LoadBayBackwards
LoadBayCurrentSpeed
LoadBayLength (Transporter)
LoadBayDeceleration
LoadBaySpeed (Transporter)
LoadBaySpeedCtrl
LoadBayType
Pause (Transporter)
RotationSpeed
RouteWeightingAttr (Transporter)
RoutingCtrl
ShiftCalendarObject (Transporter)
Speed (Transporter)
SpeedCtrl (Transporter)
StartDelayDuration
TargetDistance
TargetPosition
XDim (Transporter)
YDim (Transporter)
ZDim (Transporter)