Position
Syntax
<Path>.Position:length[3] |
The attribute Position sets the position of the graphic designated by <Path>.
Note:
When you assign the attribute, Plant Simulation deactivates graphic inheritance.
Note:
You cannot assign the attribute when the graphic is located in an automatically generated graphic group.
Data Type of the Value You Can Assign
You can assign an array of data type length with three values.
Example
obj._3D.getGraphic("default", [1,7]).Position := [5,-5,0] |
var p : length[3] := obj._3D.getGraphic("deco", [1,7]).Position |
Related Topic
Edit 3D Properties > Tab Transformation > Settings for the Position
Related Topics
Detailed Access To GraphicsaddGraphicTransformation
deleteGraphic
graphic
groupGraphics
Index
InternalGraphicType
makeAnimatableObject
MaterialActive
MaterialAmbientColor
MaterialDiffuseColor
MaterialEmissiveColor
MaterialShininess
MaterialSpecularColor
MaterialTransparency
Name
NumGraphics
ObstacleForWorker
optimizeByPruningTinyGraphics
optimizeByStructureFlattening
optimizeByVisibilityFilter
Rotation
Scale
TransformationMatrix
ungroupGraphic