Dataset ID and Dataset Revision IDs are managed during the Save process.
The Create JT option must be toggled on to save
and convert documents to JT in Teamcenter's Save Manager.
A warning message displays if the conversion process failed. Refer to the Troubleshooting section for further information, if necessary.
The created JT files display in the Updated files list window at the
end of the Save process when the catia2jt.bat/catia2jt.sh scripts are
used during conversion process
Alternate Shape Representations in a CATIA assembly do not display in the Save Manager when JT Preferences are set to create JTs for Alternate Shape Representations.
For example, CATShapes are not listed in the Save Manager below. However,
Alternate Shape Representations and their JT files are listed in the Updated
files list; JT files are listed when the conversion is performed using
the catia2jt.bat/catia2jt.sh script.