Using a Translator
Teamcenter
Translator - Dispatcher Services Method |
Installation
Topics: Theorem/Teamcenter
Translator (JT)
|
The JT conversion processes uses translators, such as a Theorem translator or a Teamcenter translator. The translator is called in the catia2jt script, so it is necessary that the script must be configured correctly.
Translate CATIA files into JTs using one of the following methods.
The catia2jt script must be configured to use with the translator specific to your environment, unless the Dispatcher Services method is used.