When a Theorem or Teamcenter translator is not used, a catia2jt script must be created adhering to the following rules.
exit 0
)exit 10
)First input parameter | Second parameter | Third parameter | |
---|---|---|---|
0 | product file name with full filepath | output directory | The created JT must exist in the output directory |
1 | directory which contains V4 files | ||
not 0 or 1 | directory which contains V5 files |